This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AL-Q1: SBL boot failed

Part Number: TDA4AL-Q1

Hi,

   We used SBL mode and replaced the APP file with AutoSAR package.But the startup failed with the following log.

   However, AutoSAR packages can be run directly through the CCS debugger.

[17:54:41:475] SBL Revision: 01.00.10.01 (Sep 26 2023 - 19:30:50)␍␍␊
[17:54:41:698] TIFS  ver: 8.6.3--v08.06.03 (Chill Capybar␍␍␊
[17:54:41:746] SCISERVER Board Configuration header population... PASSED␍␍␊
[17:54:41:810] Sciclient_setBoardConfigHeader... PASSED␍␍␊
[17:54:41:842] Initlialzing PLLs ...done.␍␍␊
[17:54:41:874] InitlialzingClocks ...done.␍␍␊
[17:54:41:906] Initlialzing DDR ...done.␍␍␊
[17:54:41:970] Initializing GTC ...Begin parsing user application␍␍␊
[17:54:42:018] Calling Sciclient_procBootRequestProcessor, ProcId 0x20... ␍␍␊
[17:54:42:082] Calling Sciclient_procBootRequestProcessor, ProcId 0x21... ␍␍␊
[17:54:42:146] Calling Sciclient_procBootRequestProcessor, ProcId 0x1... ␍␍␊
[17:54:42:210] Calling Sciclient_procBootRequestProcessor, ProcId 0x2... ␍␍␊
[17:54:42:273] Calling Sciclient_procBootRequestProcessor, ProcId 0x6... ␍␍␊
[17:54:42:321] Calling Sciclient_procBootRequestProcessor, ProcId 0x7... ␍␍␊
[17:54:42:385] Calling Sciclient_procBootRequestProcessor, ProcId 0x8... ␍␍␊
[17:54:42:449] Calling Sciclient_procBootRequestProcessor, ProcId 0x9... ␍␍␊
[17:54:42:513] Calling Sciclient_procBootRequestProcessor, ProcId 0x30... ␍␍␊
[17:54:42:561] Calling Sciclient_procBootRequestProcessor, ProcId 0x31... ␍␍␊
[17:54:42:625] Calling Sciclient_procBootRequestProcessor, ProcId 0x80... ␍␍␊
[17:54:42:769] Searching for X509 certificate ...found @0x41c7fb3c, size = 1746 bytes␍␍␍␊
[17:54:42:833] SBL reserved memory Found: Start = @ 0xc2000000, Size = 0x4000000␍␍␍␊
[17:54:42:912] Copying 1748 bytes from app to 0xc2000002␍␍␍␊
[17:54:42:960] Found seq @ 0xc200043d␍␍␍␊
[17:54:42:976] image length = 261428 bytes␍␍␍␊
[17:54:43:008] Copying 261432 bytes from offset 0x6d0 to 0xc20006d2...Cert @ 0xc2000002 ...Ignored on GP...done␍␍␍␊
[17:54:43:232] Switching core id 8, proc_id 0x1 to split mode... ␍␍␊
[17:54:43:280] Calling Sciclient_procBootGetProcessorState, ProcId 0x1... ␍␍␊
[17:54:43:344] Sciclient_procBootSetProcessorCfg, ProcId 0x1, enabling split mode...␍␍␊
[17:54:43:424] Calling Sciclient_procBootGetProcessorState, ProcId 0x1... ␍␍␊
[17:54:43:487] Enabling MCU TCMs after reset for core 8␍␍␊
[17:54:43:519] Disabling HW-based memory init of MCU TCMs for core 8␍␍␊
[17:54:43:583] Sciclient_procBootSetProcessorCfg update TCM enable/disable settings...␍␍␊
[17:54:43:647] Copying 0x40 bytes to 0x0␍␍␊
[17:54:43:679] Copying 0x444 bytes to 0x41cc0000␍␍␊
[17:54:43:711] Copying 0x314 bytes to 0x41cc1c44␍␍␊
[17:54:43:759] Copying 0x108 bytes to 0x41cc1f58␍␍␊
[17:54:43:791] Copying 0x8e8 bytes to 0x41cc2060␍␍␊
[17:54:43:823] Copying 0x11c44 bytes to 0x97000000␍␍␊
[17:54:43:855] Copying 0xd05c bytes to 0x97011c50␍␍␊
[17:54:43:903] Copying 0xbe6c bytes to 0x9701ecb0␍␍␊
[17:54:43:935] Copying 0x6134 bytes to 0x9702ab20␍␍␊
[17:54:43:967] Copying 0x45d4 bytes to 0x97035230␍␍␊
[17:54:44:015] Copying 0x41ac bytes to 0x97039804␍␍␊
[17:54:44:047] Copying 0x3fe8 bytes to 0x9703d9b0␍␍␊
[17:54:44:078] Copying 0x34 bytes to 0x970445a0␍␍␊
[17:54:44:110] Copying 0x8 bytes to 0x970445d4␍␍␊
[17:54:44:142] Copying 0x9e8 bytes to 0x97049450␍␍␊
[17:54:44:190] Copying 0x800 bytes to 0x9704a660␍␍␊
[17:54:44:222] Copying 0x458 bytes to 0x9704ae60␍␍␊
[17:54:44:254] Setting entry point for core 8 @0x41cc1f58␍␍␊
[17:54:44:302] Sciclient_procBootReleaseProcessor, ProcId 0x20...␍␍␊
[17:54:44:350] Sciclient_procBootReleaseProcessor, ProcId 0x21...␍␍␊
[17:54:44:398] Sciclient_procBootReleaseProcessor, ProcId 0x1...␍␍␊
[17:54:44:462] Sciclient_procBootReleaseProcessor, ProcId 0x2...␍␍␊
[17:54:44:510] Sciclient_procBootReleaseProcessor, ProcId 0x6...␍␍␊
[17:54:44:558] Sciclient_procBootReleaseProcessor, ProcId 0x7...␍␍␊
[17:54:44:606] Sciclient_procBootReleaseProcessor, ProcId 0x8...␍␍␊
[17:54:44:654] Sciclient_procBootReleaseProcessor, ProcId 0x9...␍␍␊
[17:54:44:717] Sciclient_procBootReleaseProcessor, ProcId 0x30...␍␍␊
[17:54:44:765] Sciclient_procBootReleaseProcessor, ProcId 0x31...␍␍␊
[17:54:44:813] Sciclient_procBootReleaseProcessor, ProcId 0x80...␍␍␊
[17:54:44:861] Calling Sciclient_procBootRequestProcessor, ProcId 0x1... ␍␍␊
[17:54:44:925] Sciclient_procBootSetProcessorCfg, ProcId 0x1, EntryPoint 0x41cc1f58...␍␍␊
[17:54:45:005] Sciclient_procBootSetProcessorCfg...FAILED