Part Number: TDA4AL-Q1
Hi,
We used SBL mode and replaced the APP file with AutoSAR package.But the startup failed with the following log.
However, AutoSAR packages can be run directly through the CCS debugger.
[17:54:41:475] SBL Revision: 01.00.10.01 (Sep 26 2023 - 19:30:50)␍␍␊ [17:54:41:698] TIFS ver: 8.6.3--v08.06.03 (Chill Capybar␍␍␊ [17:54:41:746] SCISERVER Board Configuration header population... PASSED␍␍␊ [17:54:41:810] Sciclient_setBoardConfigHeader... PASSED␍␍␊ [17:54:41:842] Initlialzing PLLs ...done.␍␍␊ [17:54:41:874] InitlialzingClocks ...done.␍␍␊ [17:54:41:906] Initlialzing DDR ...done.␍␍␊ [17:54:41:970] Initializing GTC ...Begin parsing user application␍␍␊ [17:54:42:018] Calling Sciclient_procBootRequestProcessor, ProcId 0x20... ␍␍␊ [17:54:42:082] Calling Sciclient_procBootRequestProcessor, ProcId 0x21... ␍␍␊ [17:54:42:146] Calling Sciclient_procBootRequestProcessor, ProcId 0x1... ␍␍␊ [17:54:42:210] Calling Sciclient_procBootRequestProcessor, ProcId 0x2... ␍␍␊ [17:54:42:273] Calling Sciclient_procBootRequestProcessor, ProcId 0x6... ␍␍␊ [17:54:42:321] Calling Sciclient_procBootRequestProcessor, ProcId 0x7... ␍␍␊ [17:54:42:385] Calling Sciclient_procBootRequestProcessor, ProcId 0x8... ␍␍␊ [17:54:42:449] Calling Sciclient_procBootRequestProcessor, ProcId 0x9... ␍␍␊ [17:54:42:513] Calling Sciclient_procBootRequestProcessor, ProcId 0x30... ␍␍␊ [17:54:42:561] Calling Sciclient_procBootRequestProcessor, ProcId 0x31... ␍␍␊ [17:54:42:625] Calling Sciclient_procBootRequestProcessor, ProcId 0x80... ␍␍␊ [17:54:42:769] Searching for X509 certificate ...found @0x41c7fb3c, size = 1746 bytes␍␍␍␊ [17:54:42:833] SBL reserved memory Found: Start = @ 0xc2000000, Size = 0x4000000␍␍␍␊ [17:54:42:912] Copying 1748 bytes from app to 0xc2000002␍␍␍␊ [17:54:42:960] Found seq @ 0xc200043d␍␍␍␊ [17:54:42:976] image length = 261428 bytes␍␍␍␊ [17:54:43:008] Copying 261432 bytes from offset 0x6d0 to 0xc20006d2...Cert @ 0xc2000002 ...Ignored on GP...done␍␍␍␊ [17:54:43:232] Switching core id 8, proc_id 0x1 to split mode... ␍␍␊ [17:54:43:280] Calling Sciclient_procBootGetProcessorState, ProcId 0x1... ␍␍␊ [17:54:43:344] Sciclient_procBootSetProcessorCfg, ProcId 0x1, enabling split mode...␍␍␊ [17:54:43:424] Calling Sciclient_procBootGetProcessorState, ProcId 0x1... ␍␍␊ [17:54:43:487] Enabling MCU TCMs after reset for core 8␍␍␊ [17:54:43:519] Disabling HW-based memory init of MCU TCMs for core 8␍␍␊ [17:54:43:583] Sciclient_procBootSetProcessorCfg update TCM enable/disable settings...␍␍␊ [17:54:43:647] Copying 0x40 bytes to 0x0␍␍␊ [17:54:43:679] Copying 0x444 bytes to 0x41cc0000␍␍␊ [17:54:43:711] Copying 0x314 bytes to 0x41cc1c44␍␍␊ [17:54:43:759] Copying 0x108 bytes to 0x41cc1f58␍␍␊ [17:54:43:791] Copying 0x8e8 bytes to 0x41cc2060␍␍␊ [17:54:43:823] Copying 0x11c44 bytes to 0x97000000␍␍␊ [17:54:43:855] Copying 0xd05c bytes to 0x97011c50␍␍␊ [17:54:43:903] Copying 0xbe6c bytes to 0x9701ecb0␍␍␊ [17:54:43:935] Copying 0x6134 bytes to 0x9702ab20␍␍␊ [17:54:43:967] Copying 0x45d4 bytes to 0x97035230␍␍␊ [17:54:44:015] Copying 0x41ac bytes to 0x97039804␍␍␊ [17:54:44:047] Copying 0x3fe8 bytes to 0x9703d9b0␍␍␊ [17:54:44:078] Copying 0x34 bytes to 0x970445a0␍␍␊ [17:54:44:110] Copying 0x8 bytes to 0x970445d4␍␍␊ [17:54:44:142] Copying 0x9e8 bytes to 0x97049450␍␍␊ [17:54:44:190] Copying 0x800 bytes to 0x9704a660␍␍␊ [17:54:44:222] Copying 0x458 bytes to 0x9704ae60␍␍␊ [17:54:44:254] Setting entry point for core 8 @0x41cc1f58␍␍␊ [17:54:44:302] Sciclient_procBootReleaseProcessor, ProcId 0x20...␍␍␊ [17:54:44:350] Sciclient_procBootReleaseProcessor, ProcId 0x21...␍␍␊ [17:54:44:398] Sciclient_procBootReleaseProcessor, ProcId 0x1...␍␍␊ [17:54:44:462] Sciclient_procBootReleaseProcessor, ProcId 0x2...␍␍␊ [17:54:44:510] Sciclient_procBootReleaseProcessor, ProcId 0x6...␍␍␊ [17:54:44:558] Sciclient_procBootReleaseProcessor, ProcId 0x7...␍␍␊ [17:54:44:606] Sciclient_procBootReleaseProcessor, ProcId 0x8...␍␍␊ [17:54:44:654] Sciclient_procBootReleaseProcessor, ProcId 0x9...␍␍␊ [17:54:44:717] Sciclient_procBootReleaseProcessor, ProcId 0x30...␍␍␊ [17:54:44:765] Sciclient_procBootReleaseProcessor, ProcId 0x31...␍␍␊ [17:54:44:813] Sciclient_procBootReleaseProcessor, ProcId 0x80...␍␍␊ [17:54:44:861] Calling Sciclient_procBootRequestProcessor, ProcId 0x1... ␍␍␊ [17:54:44:925] Sciclient_procBootSetProcessorCfg, ProcId 0x1, EntryPoint 0x41cc1f58...␍␍␊ [17:54:45:005] Sciclient_procBootSetProcessorCfg...FAILED