This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62A: am62a+imx623

Part Number: PROCESSOR-SDK-AM62A


Hi TI experts,

 I am debugging  AM62a+imx623 ,I have configured the ip, and ping the ip is OK, but the DCC tool cannot read registers and take pictures ,the DCC  tool version is 2.5 ,so i can't continue tune the image IQ .Please help me find the root cause ,thanks.

Besr Regards,

Renhui

  • Hello,

    Based on the given information, it is difficult to determine the root cause of the issue. However, it is possible that the problem lies with the DCC tool version being used. It may not be compatible with the AM62a+imx623 configuration. Additionally, you may want to check if there are any firmware or driver updates available for your hardware configuration.

    Regards,

    Gary

  • Hi Gary,

    What is the corret DCC version  for AM62a+imx623 so that I can apply for the DCC tool,thanks

  • I also test  am62a+imx390 and it can't read the register and capture raw/yuv.

  • Hello, please wait a moment

  • Hello,

    The correct DCC (Device Configuration Compiler) version for AM62a+imx623 depends on the specific software and development environment you are using.

    DCC is a tool provided by Texas Instruments (TI) for configuring the device-specific settings in their processors. To obtain the correct version of DCC, you should refer to the documentation and software resources provided by TI for the AM62a+imx623 platform.

    Here are some general steps to find the correct DCC version:

    1. Visit the official TI website (www.ti.com) and navigate to the product page for the AM62a+imx623 platform.

    2. Look for the software and development resources section on the product page. TI usually provides software development kits (SDKs) and other resources for their platforms.

    3. Download the SDK or software package for the AM62a+imx623 platform. This package may include the appropriate version of DCC or provide instructions on where to obtain it.

    4. Check the documentation or release notes provided with the SDK or software package. These documents should specify the required version of DCC or provide guidance on where to find it.

    5. If you are a TI customer or partner, you may also have access to additional resources and support channels. You can reach out to TI directly for assistance in obtaining the correct version of DCC for your specific use case.

    Remember that the specific version of DCC may vary depending on the software and development environment you are using. It is important to consult the official documentation and resources provided by TI for the AM62a+imx623 platform to ensure you have the correct version of DCC.

    I hope this helps! If you have any further questions, please feel free to ask.

    Regards,

    Gary

  • Hello,

    If you are having trouble reading registers or capturing raw/yuv data on the AM62a+imx390 platform, there are several things you can try to troubleshoot the issue:

    1. Check the hardware connections: Ensure that all hardware connections are properly made and that the AM62a and imx390 are correctly communicating with each other. Double-check the wiring and make sure that the power supply and clock signals are stable and within the required specifications.

    2. Check the software configuration: Make sure that the software configuration is correct and that the correct drivers and settings are being used. Check that the software is correctly configured to communicate with the imx390 and that the correct registers are being read or written.

    3. Check the software version: Make sure that you are using the correct version of the software for the AM62a+imx390 platform. Check the release notes and documentation to ensure that the software is compatible with your specific hardware and that there are no known issues or bugs that could be causing the problem.

    4. Check for errors and debug messages: Check for any error messages or debug output from the software that could provide more information about the problem. Look for any error codes or messages that indicate a problem with the hardware or software configuration.

    I hope this helps you troubleshoot the issue. If you have any further questions, please feel free to ask.

    Regards,

    Gary

  • Hi Gary,

    Thank you for your help. I will try to solve this problem according to your suggestion. Thank you!

    Best Regards,

    Renhui

  • Hello,

    Okay, feel free to communicate if you have any questions. Thank you!

    Regards,

    Gary