Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM,
关于TDA4VM上C66X的调试有几个问题麻烦咨询以下,目前前提是我计划只用到TDA4VM的MCU和C66X,其他部分内核包括A72不会用到:
1.SK-TDA4VM上的C66X的LOG输出是不是UART1,如果不是的话是哪个?
2.如果C66X的LOG输出没有配置uart口,那如何来配置?有没有案例代码?
3.C66X的SPI通讯是否支持DMA,有没有案例代码?
4.C66X和MCU2或者MCU3是否可以有内存共享地址,可以直接进行数据获取。如果没有,C66X和MCU之间如何进行通讯最高效?
5.SDK里有没有直接可以导入到CCS里的C66X的案例工程代码,经过CCS编译后可以直接加载进去后跑起来的?
6.如果没有直接导入CCS的工程代案例代码,我如何开始独立开发C66X的软件?