Part Number: SK-TDA4VM
Other Parts Discussed in Thread: TDA4VM,
关于TDA4VM上MCU的调试有几个问题麻烦咨询以下,目前前提是我计划只用到TDA4VM的MCU和C66X,MCU作为数据采集,给到DSP做运算,然后数据通过MCU存储到EMMC里,其他部分内核包括A72不会用到:
1.SK-TDA4VM上的的MCU_UART0是配置给MCU1_0来做LOG输出的吧,如果我用在MCU2_0来做log输出的UART口,如何来配置?
2.MCU2/MCU3的SPI通讯是否支持DMA,有没有案例代码?
3.SDK里有没有直接可以导入到CCS里的MCU2/MCU3的案例工程代码,经过CCS编译后可以直接加载进去后跑起来的?
4.如果没有直接导入CCS的工程代案例代码,我如何开始独立开发MCU2/MCU3的软件,比如创建一个工程代码需要引入那些库,头文件,怎么来配置等等?
5.SDK里好像都是基于freeRTOS或者safeRTOS,我想了解这两个和TI-RTOS的区别
6.MCU2/MCU3是否支持EMMC和网口,如果支持,有没有案例代码如何配置和使用的?