本人是使用appro DM368的开发机
使用RS232串口透过TFTP与终端机指令进行烧入
但是档案或位置似乎不对
现在重新上电终端机上完全没讯息
ubl的部分应该挂了
请问要如何回復?现在手边只有RS232连接debug boaed
要重烧回復的话哪边有相关文章可参考?
有看到说利用SD卡 将debug boead jp2接起来启动(但目前手边的SDHC无法使用)
也看不太懂他的步骤7) Run this command export PATH=$PATH:./bin.x86 这是在哪边输入执行?
终端机直接打执行後make有问题
#make
Command 'make' is available in '/usr/bin/make'
The command could not be located because '/usr/bin' is not included in the PATH environment variable.
make: command not found