This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J721E: 我试图使用该SDK的编译器交叉编译Boost 1_74_0库,但是Cxx11的所有feature都没有通过

  • 如果您在使用PROCESSOR-SDK-J721E的编译器交叉编译Boost库时,C++11的所有特性都没有通过,可能是由于以下原因:

    1. 编译器版本:请确保您使用的PROCESSOR-SDK-J721E的编译器版本支持C++11特性。

    2. 编译器选项:在使用PROCESSOR-SDK-J721E的编译器编译Boost库时,可能需要设置适当的编译器选项,以启用C++11特性。

    3. 环境变量:确保在编译Boost库之前,正确设置了与PROCESSOR-SDK-J721E的编译器相关的环境变量。这可能包括设置`CC`和`CXX`环境变量,以指定正确的编译器路径和名称。

    4. 头文件包含路径:在编译Boost库时,确保设置了正确的C++11标准的头文件包含路径。

    5. 链接选项:在链接Boost库时,可能需要设置适当的链接选项,以确保C++11特性能够正确链接到最终的可执行文件中。

    6. 编译器配置文件:某些情况下,您可能需要为交叉编译环境配置特定的编译器配置文件,以确保C++11特性能够正确地被编译器识别和支持。