This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
有一个项目用到C6748和TI的SN74LVC2T45MDCTTEP的芯片,如下是原理图,想用C6748的GPIO控制SN74LVC2T45MDCTTEP这个芯片,如果C6748和SN74LVC2T45MDCTTEP正常供电,C6748的GPIO能正常的控制SN74LVC2T45MDCTTEP的A1,A2脚的高低,但是我现在有一个应用场景,如下:
不给C6748供电,但是SN74LVC2T45MDCTTEP正常供电,并且SN74LVC2T45MDCTTEP的A1,A2脚上拉到3.3V,SN74LVC2T45MDCTTEP的B1,B2脚始终为低,是不是因为C6748的GPIO口有很大的下拉电阻的原因?还是由于不给C6748供电的原因,所有的GPIO口会强制拉低的原因,所以SN74LVC2T45MDCTTEP的A1,A2脚会被强制拉低,从而SN74LVC2T45MDCTTEP的B1,B2脚始终为低?谢谢
在大多数情况下,当微控制器(如C6748)未供电时,其GPIO口会处于高阻态(High-Z)状态,即不会对外部电路产生影响。但是,有些微控制器在未供电时可能会有内部电阻或保护电路导致GPIO口被强制拉低,这可能会导致您观察到的现象。
为了解决这个问题,您可以尝试在C6748未供电的情况下测量其GPIO口的状态,以确定其是否被强制拉低。
另外,为了确保SN74LVC2T45MDCTTEP的A1、A2脚在C6748未供电时能够保持在3.3V,您可以考虑使用外部上拉电阻来确保A1、A2脚的电平。这样即使C6748未供电,A1、A2脚也能够保持在3.3V,从而确保SN74LVC2T45MDCTTEP的B1、B2脚能够保持在低电平。