This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: why cannot use XDS200 connect to AM62A7?

Part Number: AM62A7


Hi,

I use this debug setup , and click "Test Connection", but failed. The log is as follows:

[Start: Texas Instruments XDS2xx USB Debug Probe_0]

 

Execute the command:

 

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

 

[Result]

 

 

-----[Print the board config pathname(s)]------------------------------------

 

C:\Users\JINGZH~1\AppData\Local\TEXASI~1\
    CCS\ccs1240\0\0\BrdDat\testBoard.dat

 

-----[Print the reset-command software log-file]-----------------------------

 

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Jun  2 2023'.
The library build time was '17:37:16'.
The library package version is '9.12.0.00150'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

 

-----[Print the reset-command hardware log-file]-----------------------------

 

This emulator does not create a reset log-file.

 

-----[An error has occurred and this utility has aborted]--------------------

 

This error is generated by TI's USCIF driver or utilities.

 

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

 

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

 

[End: Texas Instruments XDS2xx USB Debug Probe_0]

Do you know the problem? By the way, how to slow down the speed of XDS200?