Part Number: AM62A7
hi
请问一下怎 样在开发板中支持串行解串器ub954-ub953+sensor(这个不用i2c控制)
ub954是
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请参考下面,让我知道这是否有帮助。
https://www.ti.com/lit/ug/snlu224d/snlu224d.pdf
https://dev.ti.com/tirex/explore/node?node=A__ATmvgyzeqCfCvoHoyFGZGw__AM62A-ACADEMY__WeZ9SsL__LATEST
我知道SDK支持u954或融合板。
除此之外:
我们这边读相应csi寄存器
CSI_RX_IF_VBUS2APB_INTEGRATION_DEBUG
devmem2 0x30101060
/dev/mem opened.
Memory mapped at address 0xffff891ae000.
Read at address 0x30101060 (0xffff891ae060): 0x10000000
bit31-28始终是1表示当前状态WAIT_FOR_PACKET
我们发现在VH平台(这款camera sensor+ds953+ds960调通过)
如下 VH bit1-0是2,表示当前状态PAYLOAD_DATA
devmem2 0x04504060
/dev/mem opened.
Memory mapped at address 0xffffb1015000.
Read at address 0x04504060 (0xffffb1015060): 0x20000000
硬件上均为ti evm板,如下6脚量到有波形,波形与VH调的一致

接法

UB954-Q1 EVM有两个Samtec MIPI连接器,一个在顶部,一个在底部。您正在使用的一个在底部显示在您的图片。要使用这个,您需要填充如下所示的零欧姆电阻(来自UB954-Q1 EVM用户指南)。


另一种方法是在顶部使用Samtec连接器,而不填充这些电阻,如下所述:
配置UB954-Q1 EVM:
配置J16报头选择3.3v
短跳线J23使用0x3d为I2C地址

使用此连接AM62A SK到UB954-Q1 EVM:https://mou.sr/3jYCoP0

在没有得到你们回复时,我做了一下测试(没有sensor驱动的情况),如下,
v4l2-ctl -V --device /dev/video2 --stream-mmap --stream-to=frame.raw --stream-count=1
Format Video Capture:
Width/Height : 640/480
Pixel Format : 'UYVY' (UYVY 4:2:2)
Field : Any
Bytes per Line : 1280
Size Image : 614400
Colorspace : sRGB
Transfer Function : Default (maps to sRGB)
YCbCr/HSV Encoding: Default (maps to ITU-R 601)
Quantization : Default (maps to Limited Range)
Flags :
[ 39.739495] cdns-mipi-dphy 30110000.phy: DPHY wait for lane ready timeout
[ 39.746300] cdns-csi2rx 30101000.csi-bridge: Failed to configure external DPHY: -110
VIDIOC_STREAMON returned -1 (Connection timed out)
39.739495] cdns-mipi-dphy 30110000.phy: DPHY wait for lane ready timeout
[ 39.746300] cdns-csi2rx 30101000.csi-bridge: Failed to configure external DPHY: -110
VIDIOC_STREAMON returned -1 (Connection timed out)
dphy驱动有问题?
我的sdk版本号
ti-processor-sdk-linux-am62axx-evm-08.06.00.45
参考AM62A Linux SDK中的IMX390传感器驱动、UB953/960 SerDes驱动、CSI驱动代码:
有几个问题想咨询:
1.
这个代码替换到我的sdk对应ti-processor-sdk-linux-am62axx-evm-08.06.00.45路径上有很多报错
还是我不用管这个代码,只需要用自带sdk ti-processor-sdk-linux-am62axx-evm-08.06.00.45的对应文件
2.
我这边用
3.2.2.2. CSI2RX — Processor SDK AM62Ax Documentation
setenv name_overlays k3-am62a7-sk-csi2-imx219.dtbo,将
ti-processor-sdk-linux-am62axx-evm-08.06.00.45\board-support\linux-kernel\drivers\media\i2c\imx219.c,将i2c默认成功,从而生成video2等相关节点
git diff board-support/linux-kernel/drivers/media/i2c/imx219.c
diff --git a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx219.c b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx219.c
index 0c1ac2ee7..4ddc125cf 100644
--- a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx219.c
+++ b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx219.c
@@ -623,7 +623,7 @@ static int imx219_write_reg(struct imx219 *imx219, u16 reg, u32 len, u32 val)
put_unaligned_be16(reg, buf);
put_unaligned_be32(val << (8 * (4 - len)), buf + 2);
if (i2c_master_send(client, buf, len + 2) != len + 2)
- return -EIO;
+ return 0;
return 0;
}
@@ -638,6 +638,7 @@ static int imx219_write_regs(struct imx219 *imx219,
for (i = 0; i < len; i++) {
ret = imx219_write_reg(imx219, regs[i].address, 1, regs[i].val);
+ ret = 0;
if (ret) {
dev_err_ratelimited(&client->dev,
"Failed to write reg 0x%4.4x. error = %d\n",
@@ -1520,11 +1521,11 @@ static int imx219_probe(struct i2c_client *client)
ret = imx219_power_on(dev);
if (ret)
return ret;
-
+#if 0
ret = imx219_identify_module(imx219);
if (ret)
goto error_power_off;
-
+#endif
/* Set default mode to max resolution */
imx219->mode = &supported_modes[0];
gst-launch-1.0 v4l2src device=/dev/video2 io-mode=5 ! video/x-raw,width=1920,height=1080,format=YUY2 ! kmssink driver-name=tidss sync=false
发现报错了
root@am62axx-evm:/opt/edgeai-gst-apps# gst-launch-1.0 v4l2src device=/dev/video2 io-mode=5 ! video/x-raw,width=1920,height=1080,format=YUY2 ! kmssink driver-name=tidss sync=false Setting pipeline to PAUSED ... Pipeline is live and does not need PREROLL ... Setting pipeline to PLAYING ... New clock: GstSystemClock [ 2774.318781] cdns-mipi-dphy 30110000.phy: DPHY wait for lane ready timeout [ 2774.325592] cdns-csi2rx 30101000.csi-bridge: Failed to configure external DPHY: -110 ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory. Additional debug info: ../gst-plugins-good-1.16.3/sys/v4l2/gstv4l2src.c(660): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Buffer pool activation failed Execution ended after 0:00:00.124108960 Setting pipeline to NULL ... Freeing pipeline ... root@am62axx-evm:/opt/edgeai-gst-apps# root@am62axx-evm:/opt/edgeai-gst-apps# root@am62axx-evm:/opt/edgeai-gst-apps# root@am62axx-evm:/opt/edgeai-gst-apps# root@am62axx-evm:/opt/edgeai-gst-apps# gst-launch-1.0 v4l2src device=/dev/video2 io-mode=5 ! video/x-raw,width=1920,height=1080,format=YUY2 ! kmssink driver-name=tidss sync=false Setting pipeline to PAUSED ... Pipeline is live and does not need PREROLL ... Setting pipeline to PLAYING ... New clock: GstSystemClock [ 2775.712926] cdns-mipi-dphy 30110000.phy: DPHY wait for lane ready timeout [ 2775.719726] cdns-csi2rx 30101000.csi-bridge: Failed to configure external DPHY: -110 ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory. Additional debug info: ../gst-plugins-good-1.16.3/sys/v4l2/gstv4l2src.c(660): gst_v4l2src_decide_allocation (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Buffer pool activation failed Execution ended after 0:00:00.124354480 Setting pipeline to NULL ... Freeing pipeline ...这个dphy报错是驱动有问题嘛
那第二点先不提
按你们的方法来,似乎imx319报错,造成vide节点只有video0 video1
因为这边的sensor带isp,不需要控制
[ 5.623867] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xe [ 6.168223] cdns-csi2rx 30101000.csi-bridge: Probed CSI2RX with 4/4 lanes, 4 streams, external D-PHY [ 6.234559] ds90ub953 4-0044: Found rev 2, mask 0 [ 6.248485] imx390 6-001a: inck rate: 27027027 Hz [ 6.293744] imx390 6-001a: imx390_read: failed to read reg 0x0330: -121 [ 6.300527] imx390: probe of 6-001a failed with error -121
root@am62axx-evm:/opt/edgeai-gst-apps# media-ctl -p
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 0 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
pad1: Source
pad2: Source
pad3: Source
pad4: Source
pad5: Source
pad6: Source
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 1 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
pad2: Source
pad3: Source
pad4: Source
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 1 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
pad1: Source
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
root@am62axx-evm:/opt/edgeai-gst-apps# v4l2-ctl --list-devices
TI-CSI2RX (platform:30102000.ticsi2rx):
/dev/media0
wave5-dec (platform:wave5-dec):
/dev/video0
wave5-enc (platform:wave5-enc):
/dev/video1
那第二点先不提
按你们的方法来,似乎imx319报错,造成video节点只有video0 video1
因为这边的sensor带isp,不需要控制
[ 5.623867] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xe [ 6.168223] cdns-csi2rx 30101000.csi-bridge: Probed CSI2RX with 4/4 lanes, 4 streams, external D-PHY [ 6.234559] ds90ub953 4-0044: Found rev 2, mask 0 [ 6.248485] imx390 6-001a: inck rate: 27027027 Hz [ 6.293744] imx390 6-001a: imx390_read: failed to read reg 0x0330: -121 [ 6.300527] imx390: probe of 6-001a failed with error -121
将imx390重命名后,仍是如此video节点只有video0 video1
root@am62axx-evm:/opt/edgeai-gst-apps# media-ctl -p
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 0 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
pad1: Source
pad2: Source
pad3: Source
pad4: Source
pad5: Source
pad6: Source
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 1 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
pad2: Source
pad3: Source
pad4: Source
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 1 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
pad1: Source
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
有些报错
[ 6.434515] ds90ub960 4-003d: RX0 STS2 error: 0x4d [ 6.439374] ds90ub960 4-003d: RX0 CSI error: 0x2 [ 7.588124] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL) [ 7.601327] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ 11.586408] ds90ub960 4-003d: RX0 STS1 error: 0x33 [ 11.591227] ds90ub960 4-003d: RX0 STS2 error: 0x6d [ 11.596065] ds90ub960 4-003d: RX0 CSI error: 0xf [ 24.930370] ds90ub960 4-003d: RX0 STS2 error: 0xc [ 24.935084] ds90ub960 4-003d: RX0 CSI error: 0x4 [ 25.474440] ds90ub960 4-003d: RX0 STS2 error: 0x6d [ 25.479265] ds90ub960 4-003d: RX0 CSI error: 0xf [ 26.018375] ds90ub960 4-003d: RX0 STS2 error: 0x4d [ 26.023259] ds90ub960 4-003d: RX0 CSI error: 0xc [ 35.266426] ds90ub960 4-003d: RX0 STS1 error: 0x33 [ 35.274267] ds90ub960 4-003d: RX0 STS2 error: 0x6d [ 35.284739] ds90ub960 4-003d: RX0 CSI error: 0xf [ 36.834375] ds90ub960 4-003d: RX0 STS2 error: 0xc [ 36.839094] ds90ub960 4-003d: RX0 CSI error: 0xc
注释掉这个报错线程后,手动执行调试的i2c命令(sensor正常输出波形)
root@am62axx-evm:/opt/edgeai-gst-apps# media-ctl -p
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 0 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
pad1: Source
pad2: Source
pad3: Source
pad4: Source
pad5: Source
pad6: Source
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 1 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
pad2: Source
pad3: Source
pad4: Source
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 1 link, 0 route)
type V4L2 subdev subtype Unknown flags 0
pad0: Sink
pad1: Source
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
root@am62axx-evm:/opt/edgeai-gst-apps# v4l2-ctl --list-devices
TI-CSI2RX (platform:30102000.ticsi2rx):
/dev/media0
wave5-dec (platform:wave5-dec):
/dev/video0
wave5-enc (platform:wave5-enc):
/dev/video1
但仍然只有2个
重新在uboot输入
1 setenv name_overlays k3-am62a7-fpdlink-sk-fusion.dtbo k3-j721e-fpdlink-imx390-rcm-0-0.dtbo
删除掉i2c,改为手动执行脚本初始化des,ser(sensor不用初始化)
--- a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.c
+++ b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.c
@@ -33,6 +33,7 @@ static int imx390_read(struct imx390 *imx390, u16 addr, u32 *val, size_t nbytes)
__le32 val_le = 0;
ret = regmap_bulk_read(imx390->regmap, addr, &val_le, nbytes);
+ ret = 0;
if (ret < 0) {
dev_err(imx390->dev, "%s: failed to read reg 0x%04x: %d\n",
__func__, addr, ret);
@@ -49,6 +50,7 @@ static int imx390_write(struct imx390 *imx390, u16 addr, u32 val, size_t nbytes)
__le32 val_le = cpu_to_le32(val);
ret = regmap_bulk_write(imx390->regmap, addr, &val_le, nbytes);
+ ret = 0;
if (ret < 0)
dev_err(imx390->dev, "%s: failed to write reg 0x%04x: %d\n",
__func__, addr, ret);
@@ -77,6 +79,7 @@ static int imx390_write_table(struct imx390 *imx390,
int ret;
ret = regmap_multi_reg_write(imx390->regmap, regs, nr_regs);
+ ret = 0;
if (ret < 0)
dev_err(imx390->dev,
"%s: failed to write reg table (%d)!\n", __func__, ret);
@@ -408,13 +411,13 @@ static int imx390_detect(struct imx390 *imx390)
ret = imx390_read(imx390, IMX390_REG_VERSION_ROM_VERSION, &id, 2);
if (ret < 0)
return ret;
-
+#if 0
if (id != IMX390_ROM_VERSION) {
dev_err(imx390->dev,
"%s: unknown chip ID 0x%04x\n", __func__, id);
return -ENODEV;
}
-
+#endif
dev_dbg(imx390->dev, "%s: detected chip ID 0x%04x\n", __func__, id);
return 0;
}
2.
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 7 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "cdns_csi2rx.30101000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "30102000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "30102000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "30102000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
pad5: Source
-> "30102000.ticsi2rx context 4":0 [ENABLED,IMMUTABLE]
pad6: Source
-> "30102000.ticsi2rx context 5":0 [ENABLED,IMMUTABLE]
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad3: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad4: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev2
routes:
0/0 -> 4/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:SRGGB12_1X12/1936x1100 field:none]
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
[stream:0 fmt:SRGGB12_1X12/1936x1100 field:none]
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev3
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:SRGGB12_1X12/1936x1100 field:none]
<- "imx390 6-001a":0 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:SRGGB12_1X12/1936x1100 field:none]
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
- entity 29: imx390 6-001a (1 pad, 1 link, 2 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev4
routes:
0/0 -> 0/0 [ACTIVE, IMMUTABLE, SOURCE]
0/0 -> 0/1 [INACTIVE, IMMUTABLE, SOURCE]
pad0: Source
[stream:0 fmt:SRGGB12_1X12/1936x1100@1/30 field:none colorspace:smpte170m]
-> "ds90ub953 4-0044":0 [ENABLED,IMMUTABLE]
- entity 35: 30102000.ticsi2rx context 0 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video2
pad0: Sink
<- "30102000.ticsi2rx":1 [ENABLED,IMMUTABLE]
- entity 41: 30102000.ticsi2rx context 1 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video3
pad0: Sink
<- "30102000.ticsi2rx":2 [ENABLED,IMMUTABLE]
- entity 47: 30102000.ticsi2rx context 2 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video4
pad0: Sink
<- "30102000.ticsi2rx":3 [ENABLED,IMMUTABLE]
- entity 53: 30102000.ticsi2rx context 3 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video5
pad0: Sink
<- "30102000.ticsi2rx":4 [ENABLED,IMMUTABLE]
- entity 59: 30102000.ticsi2rx context 4 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video6
pad0: Sink
<- "30102000.ticsi2rx":5 [ENABLED,IMMUTABLE]
- entity 65: 30102000.ticsi2rx context 5 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video7
pad0: Sink
<- "30102000.ticsi2rx":6 [ENABLED,IMMUTABLE]
root@am62axx-evm:/opt/edgeai-gst-apps# v4l2-ctl --list-devices
j721e-csi2rx (platform:30102000.ticsi2rx):
/dev/video2
/dev/video3
/dev/video4
/dev/video5
/dev/video6
/dev/video7
/dev/media0
wave5-dec (platform:wave5-dec):
/dev/video0
wave5-enc (platform:wave5-enc):
/dev/video1
3.用gst命令获取yuv数据(解串器的CSI数据应该是yuv422_8b)
gst-launch-1.0 v4l2src device=/dev/video2 io-mode=2 ! video/x-raw,width=1920,height=1080,format=YUY2 ! kmssink driver-name=tidss sync=false
4 .ctrl+z切到后到,执行
5. sh C0.sh(des,ser初始化)
6.fg切到前台,界面没有显示camera图像
7.发现中断,只有4,并没有增长,调试发现dma接收数据不正常
247: 4 0 0 0 MSI-INTA 13045760 Level 4e230000.dma-controller chan0
247: 4 0 0 0 MSI-INTA 13045760 Level 4e230000.dma-controller chan0 248: 0 0 0 0 MSI-INTA 13045761 Level 4e230000.dma-controller chan1 249: 0 0 0 0 MSI-INTA 13045762 Level 4e230000.dma-controller chan2 250: 0 0 0 0 MSI-INTA 13045763 Level 4e230000.dma-controller chan3 251: 0 0 0 0 MSI-INTA 13045764 Level 4e230000.dma-controller chan4 252: 0 0 0 0 MSI-INTA 13045765 Level 4e230000.dma-controller chan5 254: 0 0 0 0 GICv3 134 Level 8000000.ethernet
出现这种现象是我的gst-launch-1.0命令有问题嘛,还是驱动设置有问题,这边需要怎样分析,(camera sensor与厂商沟通过,从954读到的分辨率及波形正常,且这个camera在tda4 vh中点亮过)
您的gst管道有“宽度=1920,高度=1080,格式=YUY2”,但“media-ctl -p”显示“SRGGB12_1X12/1936x1100”。
请检查这个线程是否对你的用例有帮助:e2e.ti.com/.../sk-am62a-lp-debug-about-csi2rx
参考后sdk按如下修改后更新im390ko,开机后设置如下命令:
media-ctl -V '"ds90ub953 4-0044":0 [fmt:UYVY8_2X8/1920x1080 field: none]'
media-ctl -V '"ds90ub960 4-003d":0 [fmt:UYVY8_2X8/1920x1080 field: none]'
media-ctl -V '"imx390 6-001a":0 [fmt:UYVY8_2X8/1920x1080 field: none]'
diff --git a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.c b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.c
index 6c6f077c9..e91dbec45 100644
--- a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.c
+++ b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.c
@@ -33,6 +33,7 @@ static int imx390_read(struct imx390 *imx390, u16 addr, u32 *val, size_t nbytes)
__le32 val_le = 0;
ret = regmap_bulk_read(imx390->regmap, addr, &val_le, nbytes);
+ ret = 0;
if (ret < 0) {
dev_err(imx390->dev, "%s: failed to read reg 0x%04x: %d\n",
__func__, addr, ret);
@@ -49,6 +50,7 @@ static int imx390_write(struct imx390 *imx390, u16 addr, u32 val, size_t nbytes)
__le32 val_le = cpu_to_le32(val);
ret = regmap_bulk_write(imx390->regmap, addr, &val_le, nbytes);
+ ret = 0;
if (ret < 0)
dev_err(imx390->dev, "%s: failed to write reg 0x%04x: %d\n",
__func__, addr, ret);
@@ -77,6 +79,7 @@ static int imx390_write_table(struct imx390 *imx390,
int ret;
ret = regmap_multi_reg_write(imx390->regmap, regs, nr_regs);
+ ret = 0;
if (ret < 0)
dev_err(imx390->dev,
"%s: failed to write reg table (%d)!\n", __func__, ret);
@@ -88,9 +91,9 @@ static void imx390_init_formats(struct v4l2_subdev_state *state)
struct v4l2_mbus_framefmt *format;
format = v4l2_state_get_stream_format(state, 0, 0);
- format->code = imx390_mbus_formats[0];
- format->width = imx390_framesizes[0].width;
- format->height = imx390_framesizes[0].height;
+ format->code = MEDIA_BUS_FMT_UYVY8_2X8;
+ format->width = 1920;
+ format->height = 1080;
format->field = V4L2_FIELD_NONE;
format->colorspace = V4L2_COLORSPACE_SMPTE170M;
}
@@ -228,10 +231,10 @@ static int imx390_set_fmt(struct v4l2_subdev *sd,
goto done;
}
- format->code = code;
- format->width = fsize->width;
- format->height = fsize->height;
-
+ format->code = MEDIA_BUS_FMT_UYVY8_2X8;
+ format->width = 1920;//fsize->width;
+ format->height = 1080;//fsize->height;
+
fmt->format = *format;
done:
@@ -408,13 +411,13 @@ static int imx390_detect(struct imx390 *imx390)
ret = imx390_read(imx390, IMX390_REG_VERSION_ROM_VERSION, &id, 2);
if (ret < 0)
return ret;
-
+#if 0
if (id != IMX390_ROM_VERSION) {
dev_err(imx390->dev,
"%s: unknown chip ID 0x%04x\n", __func__, id);
return -ENODEV;
}
-
+#endif
dev_dbg(imx390->dev, "%s: detected chip ID 0x%04x\n", __func__, id);
return 0;
}
diff --git a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.h b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.h
index 30e518afb..71883a2cb 100644
--- a/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.h
+++ b/ti-processor-sdk-linux-am62axx-evm-08.06.00.45/board-support/linux-kernel/drivers/media/i2c/imx390.h
@@ -9,8 +9,8 @@
#include <linux/types.h>
-#define IMX390_ACTIVE_AREA_WIDTH 1936
-#define IMX390_ACTIVE_AREA_HEIGHT 1096
+#define IMX390_ACTIVE_AREA_WIDTH 1920
+#define IMX390_ACTIVE_AREA_HEIGHT 1080
/* SMPG cannot be disabled, and datatype is the same as the pixel data */
#define IMX390_SMPG_HEIGHT 4
@@ -138,7 +138,7 @@ static const struct v4l2_area imx390_framesizes[] = {
};
static const u32 imx390_mbus_formats[] = {
- MEDIA_BUS_FMT_SRGGB12_1X12,
+ MEDIA_BUS_FMT_UYVY8_2X8,
};
static const struct regmap_config imx390_regmap_config = {
(END)
media-ctl -p
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 7 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "cdns_csi2rx.30101000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "30102000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "30102000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "30102000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
pad5: Source
-> "30102000.ticsi2rx context 4":0 [ENABLED,IMMUTABLE]
pad6: Source
-> "30102000.ticsi2rx context 5":0 [ENABLED,IMMUTABLE]
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad3: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad4: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev2
routes:
0/0 -> 4/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none]
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none]
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev3
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none colorspace:smpte170m]
<- "imx390 6-001a":0 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none colorspace:smpte170m]
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
- entity 29: imx390 6-001a (1 pad, 1 link, 2 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev4
routes:
0/0 -> 0/0 [ACTIVE, IMMUTABLE, SOURCE]
0/0 -> 0/1 [INACTIVE, IMMUTABLE, SOURCE]
pad0: Source
[stream:0 fmt:UYVY8_2X8/1920x1080@1/30 field:none colorspace:smpte170m]
-> "ds90ub953 4-0044":0 [ENABLED,IMMUTABLE]
- entity 35: 30102000.ticsi2rx context 0 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video2
pad0: Sink
<- "30102000.ticsi2rx":1 [ENABLED,IMMUTABLE]
- entity 41: 30102000.ticsi2rx context 1 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video3
pad0: Sink
<- "30102000.ticsi2rx":2 [ENABLED,IMMUTABLE]
- entity 47: 30102000.ticsi2rx context 2 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video4
pad0: Sink
<- "30102000.ticsi2rx":3 [ENABLED,IMMUTABLE]
- entity 53: 30102000.ticsi2rx context 3 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video5
pad0: Sink
<- "30102000.ticsi2rx":4 [ENABLED,IMMUTABLE]
- entity 59: 30102000.ticsi2rx context 4 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video6
pad0: Sink
<- "30102000.ticsi2rx":5 [ENABLED,IMMUTABLE]
- entity 65: 30102000.ticsi2rx context 5 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video7
pad0: Sink
<- "30102000.ticsi2rx":6 [ENABLED,IMMUTABLE]
yavta -s 1920x1080 -f UYVY /dev/video2 -c100 程序没有接收到数据,卡住,中断没有增长
247: 0 0 0 0 MSI-INTA 13045760 Level 4e230000.dma-controller chan0
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -s 1920x1080 -f UYVY /dev/video2 -c100
Device /dev/video2 opened.
[ 435.326314] zyk ti_csi2rx_queue_setup 823
Device `j721e-csi2rx' on `platform:30102000.ticsi2rx' is a video[ 435.334568] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 0, plane 0 offset 0x00000000
output (without mplanes) device.
Video format set: UYVY (59565[ 435.336108] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 1, plane 0 offset 0x003f5000
955) 1920x1080 (stride 3840) field none buffer size 4147200
Vid[ 435.364383] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 2, plane 0 offset 0x007ea000
eo format: UYVY (59565955) 1920x1080 (stride 3840) field none bu[ 435.379607] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 3, plane 0 offset 0x00bdf000
ffer size 4147200
[ 435.394763] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 4, plane 0 offset 0x00fd4000
[ 435.405939] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 5, plane 0 offset 0x013c9000
[ 435.417020] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 6, plane 0 offset 0x017be000
[ 435.428252] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 7, plane 0 offset 0x01bb3000
[ 435.437962] videobuf2_common: [cap-000000009f39c6d2] __vb2_queue_alloc: allocated 8 buffers, 1 plane(s) each
8 buffers requested.
[ 435.448111] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 0, plane 0 successfully mapped
length: 4147200 offset: 0 timestamp type/source: mono/EoF
[ 435.459148] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 1, plane 0 successfully mapped
Buffer 0/0 mapped at address 0xffffbbca5000.
length: 4147200 of[ 435.473219] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 2, plane 0 successfully mapped
fset: 4149248 timestamp type/source: mono/EoF
Buffer 1/0 mapped[ 435.488002] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 3, plane 0 successfully mapped
at address 0xffffbb8b0000.
length: 4147200 offset: 8298496 tim[ 435.502529] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 4, plane 0 successfully mapped
estamp type/source: mono/EoF
Buffer 2/0 mapped at address 0xfff[ 435.517316] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 5, plane 0 successfully mapped
fbb4bb000.
length: 4147200 offset: 12447744 timestamp type/sour[ 435.531853] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 6, plane 0 successfully mapped
ce: mono/EoF
Buffer 3/0 mapped at address 0xffffbb0c6000.
leng[ 435.546641] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 7, plane 0 successfully mapped
th: 4147200 offset: 16596992 timestamp type/source: mono/EoF
Bu[ 435.561119] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 0 succeeded
ffer 4/0 mapped at address 0xffffbacd1000.
length: 4147200 offs[ 435.575323] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 1 succeeded
et: 20746240 timestamp type/source: mono/EoF
Buffer 5/0 mapped [ 435.589343] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 2 succeeded
at address 0xffffba8dc000.
length: 4147200 offset: 24895488 tim[ 435.603600] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 3 succeeded
estamp type/source: mono/EoF
Buffer 6/0 mapped at address 0xfff[ 435.617648] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 4 succeeded
fba4e7000.
length: 4147200 offset: 29044736 timestamp type/sour[ 435.617658] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 5 succeeded
ce: mono/EoF
Buffer 7/0 mapped at address 0xffffba0f2000.
[ 435.645889] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 6 succeeded
[ 435.645897] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 7 succeeded
[ 435.645908] zyk ti_csi2rx_buffer_queue 875
[ 435.672501] zyk ti_csi2rx_buffer_queue 875
[ 435.672507] zyk ti_csi2rx_buffer_queue 875
[ 435.680838] zyk ti_csi2rx_buffer_queue 875
[ 435.680844] zyk ti_csi2rx_buffer_queue 875
[ 435.689180] zyk ti_csi2rx_buffer_queue 875
[ 435.689184] zyk ti_csi2rx_buffer_queue 875
[ 435.689187] zyk ti_csi2rx_buffer_queue 875
[ 435.877773] zyk ti_csi2rx_start_dma 771
[ 435.881816] videobuf2_common: [cap-000000009f39c6d2] vb2_core_streamon: successful
[ 435.889481] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: will sleep waiting for buffers
^Z[ 437.862555] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: sleep was interrupted
[1]+ Stopped(SIGTSTP) yavta -s 1920x1080 -f UYVY /dev/video2 -c100
root@am62axx-evm:/opt/edgeai-gst-apps# sh C0.sh
953 config
953 end config
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# fg
yavta -s 1920x1080 -f UYVY /dev/video2 -c100
[ 445.513861] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: will sleep waiting for buffers
^Z[ 448.390111] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: sleep was interrupted
[1]+ Stopped(SIGTSTP) yavta -s 1920x1080 -f UYVY /dev/video2 -c100
root@am62axx-evm:/opt/edgeai-gst-apps# cat /proc/interrupts
CPU0 CPU1 CPU2 CPU3
11: 17080 19933 16119 16562 GICv3 30 Level arch_timer
14: 0 0 0 0 GICv3 23 Level arm-pmu
15: 443 0 0 0 GICv3 66 Level 4d000000.mailbox thr_012
16: 1123 0 0 0 GICv3 210 Level 2800000.serial
17: 27665 0 0 0 GICv3 193 Level 20000000.i2c
18: 380 0 0 0 GICv3 194 Level 20010000.i2c
19: 422 0 0 0 GICv3 195 Level 20020000.i2c
20: 707 0 0 0 GICv3 165 Level mmc0
21: 15798 0 0 0 GICv3 115 Level mmc1
22: 1142 0 0 0 GICv3 116 Level tidss
24: 3 0 0 0 GICv3 171 Level fc40000.spi
25: 5 0 0 0 GICv3 108 Level mbox-r5-0
26: 4 0 0 0 GICv3 109 Level mbox-c7x-0
27: 5 0 0 0 GICv3 140 Level mbox-mcu_r5-0
29: 0 0 0 0 GICv3 270 Level 2b10000.mcasp_tx
30: 0 0 0 0 GICv3 269 Level 2b10000.mcasp_rx
31: 412 0 0 0 MSI-INTA 1713152 Level 485c0100.dma-controller chan0
49: 0 0 0 0 MSI-INTA 1714176 Edge 485c0100.dma-controller chan1
61: 0 0 0 0 MSI-INTA 1714688 Level 485c0100.dma-controller chan1
79: 0 0 0 0 MSI-INTA 1715718 Edge 485c0100.dma-controller chan2
97: 0 0 0 0 MSI-INTA 1716230 Level 485c0100.dma-controller chan2
119: 0 0 0 0 MSI-INTA 1970707 Level 8000000.ethernet-tx0
191: 0 0 0 0 MSI-INTA 1970779 Level 485c0000.dma-controller chan2
209: 0 0 0 0 MSI-INTA 1971731 Level 8000000.ethernet
233: 0 0 0 0 MSI-INTA 1971755 Level 485c0000.dma-controller chan0
234: 0 0 0 0 MSI-INTA 1971756 Level 485c0000.dma-controller chan1
241: 0 0 0 0 MSI-INTA 13045248 Edge 4e230000.dma-controller chan0
242: 0 0 0 0 MSI-INTA 13045249 Edge 4e230000.dma-controller chan1
243: 0 0 0 0 MSI-INTA 13045250 Edge 4e230000.dma-controller chan2
244: 0 0 0 0 MSI-INTA 13045251 Edge 4e230000.dma-controller chan3
245: 0 0 0 0 MSI-INTA 13045252 Edge 4e230000.dma-controller chan4
246: 0 0 0 0 MSI-INTA 13045253 Edge 4e230000.dma-controller chan5
247: 0 0 0 0 MSI-INTA 13045760 Level 4e230000.dma-controller chan0
248: 0 0 0 0 MSI-INTA 13045761 Level 4e230000.dma-controller chan1
249: 0 0 0 0 MSI-INTA 13045762 Level 4e230000.dma-controller chan2
250: 0 0 0 0 MSI-INTA 13045763 Level 4e230000.dma-controller chan3
251: 0 0 0 0 MSI-INTA 13045764 Level 4e230000.dma-controller chan4
252: 0 0 0 0 MSI-INTA 13045765 Level 4e230000.dma-controller chan5
254: 0 0 0 0 GICv3 134 Level 8000000.ethernet
383: 39 0 0 0 GPIO 23 Edge -davinci_gpio 1-0022
448: 0 0 0 0 1-0022 16 Edge 1-003b
453: 0 0 0 0 GICv3 258 Level xhci-hcd:usb1
IPI0: 9077 13756 13952 12448 Rescheduling interrupts
IPI1: 611 614 389 370 Function call interrupts
IPI2: 0 0 0 0 CPU stop interrupts
IPI3: 0 0 0 0 CPU stop (for crash dump) interrupts
IPI4: 0 0 0 0 Timer broadcast interrupts
IPI5: 0 0 0 0 IRQ work interrupts
IPI6: 0 0 0 0 CPU wake-up interrupts
再来一次
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -s 1920x1080 -f UYVY /dev/video2 -c100
Device /dev/video2 opened.
[ 864.476420] zyk ti_csi2rx_queue_setup 823
Device `j721e-csi2rx' on `platform:30102000.ticsi2rx' is a video[ 864.484572] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 0, plane 0 offset 0x00000000
output (without mplanes) device.
Video format set: UYVY (59565[ 864.499613] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 1, plane 0 offset 0x003f5000
955) 1920x1080 (stride 3840) field none buffer size 4147200
Vid[ 864.514869] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 2, plane 0 offset 0x007ea000
eo format: UYVY (59565955) 1920x1080 (stride 3840) field none bu[ 864.529525] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 3, plane 0 offset 0x00bdf000
ffer size 4147200
[ 864.544838] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 4, plane 0 offset 0x00fd4000
[ 864.556105] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 5, plane 0 offset 0x013c9000
[ 864.567413] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 6, plane 0 offset 0x017be000
[ 864.578728] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 7, plane 0 offset 0x01bb3000
[ 864.588313] videobuf2_common: [cap-000000009f39c6d2] __vb2_queue_alloc: allocated 8 buffers, 1 plane(s) each
8 buffers requested.
[ 864.598703] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 0, plane 0 successfully mapped
length: 4147200 offset: 0 timestamp type/source: mono/EoF
[ 864.609786] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 1, plane 0 successfully mapped
Buffer 0/0 mapped at address 0xffffad923000.
length: 4147200 of[ 864.623787] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 2, plane 0 successfully mapped
fset: 4149248 timestamp type/source: mono/EoF
Buffer 1/0 mapped[ 864.638604] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 3, plane 0 successfully mapped
at address 0xffffad52e000.
length: 4147200 offset: 8298496 tim[ 864.653075] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 4, plane 0 successfully mapped
estamp type/source: mono/EoF
Buffer 2/0 mapped at address 0xfff[ 864.667841] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 5, plane 0 successfully mapped
fad139000.
length: 4147200 offset: 12447744 timestamp type/sour[ 864.682398] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 6, plane 0 successfully mapped
ce: mono/EoF
Buffer 3/0 mapped at address 0xffffacd44000.
leng[ 864.697161] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 7, plane 0 successfully mapped
th: 4147200 offset: 16596992 timestamp type/source: mono/EoF
Bu[ 864.711671] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 0 succeeded
ffer 4/0 mapped at address 0xffffac94f000.
length: 4147200 offs[ 864.725892] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 1 succeeded
et: 20746240 timestamp type/source: mono/EoF
Buffer 5/0 mapped [ 864.739908] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 2 succeeded
at address 0xffffac55a000.
length: 4147200 offset: 24895488 tim[ 864.754153] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 3 succeeded
estamp type/source: mono/EoF
Buffer 6/0 mapped at address 0xfff[ 864.768197] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 4 succeeded
fac165000.
length: 4147200 offset: 29044736 timestamp type/sour[ 864.768208] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 5 succeeded
ce: mono/EoF
Buffer 7/0 mapped at address 0xffffabd70000.
[ 864.796451] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 6 succeeded
[ 864.796460] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 7 succeeded
[ 864.818997] zyk ti_csi2rx_buffer_queue 875
[ 864.819001] zyk ti_csi2rx_buffer_queue 875
[ 864.819007] zyk ti_csi2rx_buffer_queue 875
[ 864.831438] zyk ti_csi2rx_buffer_queue 875
[ 864.831444] zyk ti_csi2rx_buffer_queue 875
[ 864.839786] zyk ti_csi2rx_buffer_queue 875
[ 864.839794] zyk ti_csi2rx_buffer_queue 875
[ 864.848187] zyk ti_csi2rx_buffer_queue 875
[ 865.029742] zyk ti_csi2rx_start_dma 771
[ 865.033794] videobuf2_common: [cap-000000009f39c6d2] vb2_core_streamon: successful
[ 865.041464] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: will sleep waiting for buffers
^Z[ 868.848780] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: sleep was interrupted
[1]+ Stopped(SIGTSTP) yavta -s 1920x1080 -f UYVY /dev/video2 -c100
root@am62axx-evm:/opt/edgeai-gst-apps# cat /proc/interrupts
CPU0 CPU1 CPU2 CPU3
11: 26588 31739 25419 25286 GICv3 30 Level arch_timer
14: 0 0 0 0 GICv3 23 Level arm-pmu
15: 459 0 0 0 GICv3 66 Level 4d000000.mailbox thr_012
16: 1366 0 0 0 GICv3 210 Level 2800000.serial
17: 53626 0 0 0 GICv3 193 Level 20000000.i2c
18: 380 0 0 0 GICv3 194 Level 20010000.i2c
19: 482 0 0 0 GICv3 195 Level 20020000.i2c
20: 707 0 0 0 GICv3 165 Level mmc0
21: 16014 0 0 0 GICv3 115 Level mmc1
22: 1142 0 0 0 GICv3 116 Level tidss
24: 3 0 0 0 GICv3 171 Level fc40000.spi
25: 5 0 0 0 GICv3 108 Level mbox-r5-0
26: 4 0 0 0 GICv3 109 Level mbox-c7x-0
27: 5 0 0 0 GICv3 140 Level mbox-mcu_r5-0
29: 0 0 0 0 GICv3 270 Level 2b10000.mcasp_tx
30: 0 0 0 0 GICv3 269 Level 2b10000.mcasp_rx
31: 412 0 0 0 MSI-INTA 1713152 Level 485c0100.dma-controller chan0
49: 0 0 0 0 MSI-INTA 1714176 Edge 485c0100.dma-controller chan1
61: 0 0 0 0 MSI-INTA 1714688 Level 485c0100.dma-controller chan1
79: 0 0 0 0 MSI-INTA 1715718 Edge 485c0100.dma-controller chan2
97: 0 0 0 0 MSI-INTA 1716230 Level 485c0100.dma-controller chan2
119: 0 0 0 0 MSI-INTA 1970707 Level 8000000.ethernet-tx0
191: 0 0 0 0 MSI-INTA 1970779 Level 485c0000.dma-controller chan2
209: 0 0 0 0 MSI-INTA 1971731 Level 8000000.ethernet
233: 0 0 0 0 MSI-INTA 1971755 Level 485c0000.dma-controller chan0
234: 0 0 0 0 MSI-INTA 1971756 Level 485c0000.dma-controller chan1
241: 0 0 0 0 MSI-INTA 13045248 Edge 4e230000.dma-controller chan0
242: 0 0 0 0 MSI-INTA 13045249 Edge 4e230000.dma-controller chan1
243: 0 0 0 0 MSI-INTA 13045250 Edge 4e230000.dma-controller chan2
244: 0 0 0 0 MSI-INTA 13045251 Edge 4e230000.dma-controller chan3
245: 0 0 0 0 MSI-INTA 13045252 Edge 4e230000.dma-controller chan4
246: 0 0 0 0 MSI-INTA 13045253 Edge 4e230000.dma-controller chan5
247: 2 0 0 0 MSI-INTA 13045760 Level 4e230000.dma-controller chan0
248: 0 0 0 0 MSI-INTA 13045761 Level 4e230000.dma-controller chan1
249: 0 0 0 0 MSI-INTA 13045762 Level 4e230000.dma-controller chan2
250: 0 0 0 0 MSI-INTA 13045763 Level 4e230000.dma-controller chan3
251: 0 0 0 0 MSI-INTA 13045764 Level 4e230000.dma-controller chan4
252: 0 0 0 0 MSI-INTA 13045765 Level 4e230000.dma-controller chan5
254: 0 0 0 0 GICv3 134 Level 8000000.ethernet
383: 39 0 0 0 GPIO 23 Edge -davinci_gpio 1-0022
448: 0 0 0 0 1-0022 16 Edge 1-003b
453: 0 0 0 0 GICv3 258 Level xhci-hcd:usb1
IPI0: 17485 22964 24111 22547 Rescheduling interrupts
IPI1: 928 829 612 586 Function call interrupts
IPI2: 0 0 0 0 CPU stop interrupts
IPI3: 0 0 0 0 CPU stop (for crash dump) interrupts
IPI4: 0 0 0 0 Timer broadcast interrupts
IPI5: 0 0 0 0 IRQ work interrupts
IPI6: 0 0 0 0 CPU wake-up interrupts
Err: 0
root@am62axx-evm:/opt/edgeai-gst-apps# fg
yavta -s 1920x1080 -f UYVY /dev/video2 -c100
[ 884.289851] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: will sleep waiting for buffers
yavta -c -Fcapture -s 1920x1080 -f UYVY /dev/video2
的情况
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -c -Fcapture -s 1920x1080 -f UYVY /dev/video2 Device /dev/video2 opened. [ 1457.460489] zyk ti_csi2rx_queue_setup 823 Device `j721e-csi2rx' on `platform:30102000.ticsi2rx' is a video[ 1457.468632] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 0, plane 0 offset 0x00000000 output (without mplanes) device. Video format set: UYVY (59565[ 1457.483716] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 1, plane 0 offset 0x003f5000 955) 1920x1080 (stride 3840) field none buffer size 4147200 Vid[ 1457.498863] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 2, plane 0 offset 0x007ea000 eo format: UYVY (59565955) 1920x1080 (stride 3840) field none bu[ 1457.513770] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 3, plane 0 offset 0x00bdf000 ffer size 4147200 [ 1457.528721] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 4, plane 0 offset 0x00fd4000 [ 1457.540106] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 5, plane 0 offset 0x013c9000 [ 1457.551455] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 6, plane 0 offset 0x017be000 [ 1457.562779] videobuf2_common: [cap-000000009f39c6d2] __setup_offsets: buffer 7, plane 0 offset 0x01bb3000 [ 1457.572351] videobuf2_common: [cap-000000009f39c6d2] __vb2_queue_alloc: allocated 8 buffers, 1 plane(s) each 8 buffers requested. [ 1457.582680] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 0, plane 0 successfully mapped length: 4147200 offset: 0 timestamp type/source: mono/EoF [ 1457.593594] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 1, plane 0 successfully mapped Buffer 0/0 mapped at address 0xffff957d2000. length: 4147200 of[ 1457.607725] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 2, plane 0 successfully mapped fset: 4149248 timestamp type/source: mono/EoF Buffer 1/0 mapped[ 1457.622636] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 3, plane 0 successfully mapped at address 0xffff953dd000. length: 4147200 offset: 8298496 tim[ 1457.637086] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 4, plane 0 successfully mapped estamp type/source: mono/EoF Buffer 2/0 mapped at address 0xfff[ 1457.651844] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 5, plane 0 successfully mapped f94fe8000. length: 4147200 offset: 12447744 timestamp type/sour[ 1457.666385] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 6, plane 0 successfully mapped ce: mono/EoF Buffer 3/0 mapped at address 0xffff94bf3000. leng[ 1457.681228] videobuf2_common: [cap-000000009f39c6d2] vb2_mmap: buffer 7, plane 0 successfully mapped th: 4147200 offset: 16596992 timestamp type/source: mono/EoF Bu[ 1457.695663] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 0 succeeded ffer 4/0 mapped at address 0xffff947fe000. length: 4147200 offs[ 1457.709893] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 1 succeeded et: 20746240 timestamp type/source: mono/EoF Buffer 5/0 mapped [ 1457.723899] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 2 succeeded at address 0xffff94409000. length: 4147200 offset: 24895488 tim[ 1457.738197] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 3 succeeded estamp type/source: mono/EoF Buffer 6/0 mapped at address 0xfff[ 1457.752202] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 4 succeeded f94014000. length: 4147200 offset: 29044736 timestamp type/sour[ 1457.752213] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 5 succeeded ce: mono/EoF Buffer 7/0 mapped at address 0xffff93c1f000. [ 1457.780437] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 6 succeeded [ 1457.780450] videobuf2_common: [cap-000000009f39c6d2] vb2_core_qbuf: qbuf of buffer 7 succeeded [ 1457.802997] zyk ti_csi2rx_buffer_queue 875 [ 1457.807277] zyk ti_csi2rx_buffer_queue 875 [ 1457.807281] zyk ti_csi2rx_buffer_queue 875 [ 1457.807285] zyk ti_csi2rx_buffer_queue 875 [ 1457.807288] zyk ti_csi2rx_buffer_queue 875 [ 1457.807290] zyk ti_csi2rx_buffer_queue 875 [ 1457.807299] zyk ti_csi2rx_buffer_queue 875 [ 1457.807304] zyk ti_csi2rx_buffer_queue 875 [ 1458.013750] zyk ti_csi2rx_start_dma 771 [ 1458.017812] videobuf2_common: [cap-000000009f39c6d2] vb2_core_streamon: successful [ 1458.025543] videobuf2_common: [cap-000000009f39c6d2] __vb2_wait_for_done_vb: will sleep waiting for buffers
这边也按链接的方法作了个imx390dummypad,情况也是一样,中断没增加,也没有录到图像,media-ctrl -p看format没有什么不同了
sh fmt-dummy.sh
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -s 1920x1080 -f UYVY /dev/video2 -c100^C
root@am62axx-evm:/opt/edgeai-gst-apps# media-ctl -2023 Feb 27 10:38:50 am62axx-evm Process 1172 (edgeai-gui-app) of user 0 dumped core.
2023 Feb 27 10:38:50 am62axx-evm Process 1172 (edgeai-gui-app) of user 0 dumped core.
p
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 7 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "cdns_csi2rx.30101000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "30102000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "30102000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "30102000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
pad5: Source
-> "30102000.ticsi2rx context 4":0 [ENABLED,IMMUTABLE]
pad6: Source
-> "30102000.ticsi2rx context 5":0 [ENABLED,IMMUTABLE]
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad3: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad4: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev2
routes:
0/0 -> 4/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none]
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none]
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev3
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none colorspace:smpte170m]
<- "imx390dummy 6-001a":0 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none colorspace:smpte170m]
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
- entity 29: imx390dummy 6-001a (1 pad, 1 link, 2 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev4
routes:
0/0 -> 0/0 [ACTIVE, IMMUTABLE, SOURCE]
0/0 -> 0/1 [INACTIVE, IMMUTABLE, SOURCE]
pad0: Source
[stream:0 fmt:UYVY8_2X8/1920x1080@1/30 field:none colorspace:smpte170m]
-> "ds90ub953 4-0044":0 [ENABLED,IMMUTABLE]
- entity 35: 30102000.ticsi2rx context 0 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video2
pad0: Sink
<- "30102000.ticsi2rx":1 [ENABLED,IMMUTABLE]
- entity 41: 30102000.ticsi2rx context 1 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video3
pad0: Sink
<- "30102000.ticsi2rx":2 [ENABLED,IMMUTABLE]
- entity 47: 30102000.ticsi2rx context 2 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video4
pad0: Sink
<- "30102000.ticsi2rx":3 [ENABLED,IMMUTABLE]
- entity 53: 30102000.ticsi2rx context 3 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video5
pad0: Sink
<- "30102000.ticsi2rx":4 [ENABLED,IMMUTABLE]
- entity 59: 30102000.ticsi2rx context 4 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video6
pad0: Sink
<- "30102000.ticsi2rx":5 [ENABLED,IMMUTABLE]
- entity 65: 30102000.ticsi2rx context 5 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video7
pad0: Sink
<- "30102000.ticsi2rx":6 [ENABLED,IMMUTABLE]
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -s 1920x1080 -f UYVY /dev/video2 -c100
Device /dev/video2 opened.
[ 45.194119] zyk ti_csi2rx_queue_setup 823
Device `j721e-csi2rx' on `platform:30102000.ticsi2rx' is a video[ 45.202359] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 0, plane 0 offset 0x00000000
output (without mplanes) device.
Video format set: UYVY (59565[ 45.217124] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 1, plane 0 offset 0x003f5000
955) 1920x1080 (stride 3840) field none buffer size 4147200
Vid[ 45.232340] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 2, plane 0 offset 0x007ea000
eo format: UYVY (59565955) 1920x1080 (stride 3840) field none bu[ 45.247598] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 3, plane 0 offset 0x00bdf000
ffer size 4147200
[ 45.262464] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 4, plane 0 offset 0x00fd4000
[ 45.273497] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 5, plane 0 offset 0x013c9000
[ 45.284784] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 6, plane 0 offset 0x017be000
[ 45.296014] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 7, plane 0 offset 0x01bb3000
[ 45.305733] videobuf2_common: [cap-00000000cb995559] __vb2_queue_alloc: allocated 8 buffers, 1 plane(s) each
8 buffers requested.
[ 45.315896] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 0, plane 0 successfully mapped
length: 4147200 offset: 0 timestamp type/source: mono/EoF
[ 45.326905] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 1, plane 0 successfully mapped
Buffer 0/0 mapped at address 0xffff90858000.
length: 4147200 of[ 45.340994] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 2, plane 0 successfully mapped
fset: 4149248 timestamp type/source: mono/EoF
Buffer 1/0 mapped[ 45.355768] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 3, plane 0 successfully mapped
at address 0xffff90463000.
length: 4147200 offset: 8298496 tim[ 45.370292] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 4, plane 0 successfully mapped
estamp type/source: mono/EoF
Buffer 2/0 mapped at address 0xfff[ 45.385079] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 5, plane 0 successfully mapped
f9006e000.
length: 4147200 offset: 12447744 timestamp type/sour[ 45.399614] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 6, plane 0 successfully mapped
ce: mono/EoF
Buffer 3/0 mapped at address 0xffff8fc79000.
leng[ 45.414405] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 7, plane 0 successfully mapped
th: 4147200 offset: 16596992 timestamp type/source: mono/EoF
Bu[ 45.428887] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 0 succeeded
ffer 4/0 mapped at address 0xffff8f884000.
length: 4147200 offs[ 45.443092] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 1 succeeded
et: 20746240 timestamp type/source: mono/EoF
Buffer 5/0 mapped [ 45.457113] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 2 succeeded
at address 0xffff8f48f000.
length: 4147200 offset: 24895488 tim[ 45.471343] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 3 succeeded
estamp type/source: mono/EoF
Buffer 6/0 mapped at address 0xfff[ 45.485408] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 4 succeeded
f8f09a000.
length: 4147200 offset: 29044736 timestamp type/sour[ 45.485418] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 5 succeeded
ce: mono/EoF
Buffer 7/0 mapped at address 0xffff8eca5000.
[ 45.513652] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 6 succeeded
[ 45.513664] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 7 succeeded
[ 45.536178] zyk ti_csi2rx_buffer_queue 875
[ 45.540487] zyk ti_csi2rx_buffer_queue 875
[ 45.544616] zyk ti_csi2rx_buffer_queue 875
[ 45.544622] zyk ti_csi2rx_buffer_queue 875
[ 45.552954] zyk ti_csi2rx_buffer_queue 875
[ 45.552958] zyk ti_csi2rx_buffer_queue 875
[ 45.552961] zyk ti_csi2rx_buffer_queue 875
[ 45.552963] zyk ti_csi2rx_buffer_queue 875
[ 45.570942] zyk ti_csi2rx_start_dma 771
[ 45.574949] videobuf2_common: [cap-00000000cb995559] vb2_core_streamon: successful
[ 45.582596] videobuf2_common: [cap-00000000cb995559] __vb2_wait_for_done_vb: will sleep waiting for buffers
^Z[ 48.565869] videobuf2_common: [cap-00000000cb995559] __vb2_wait_for_done_vb: sleep was interrupted
[1]+ Stopped(SIGTSTP) yavta -s 1920x1080 -f UYVY /dev/video2 -c100
root@am62axx-evm:/opt/edgeai-gst-apps# sh C0.sh
953 config
953 end config
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# fg
yavta -s 1920x1080 -f UYVY /dev/video2 -c100[ 54.197831] videobuf2_common: [cap-00000000cb995559] __vb2_wait_for_done_vb: will sleep waiting for buffers
这边也按链接的方法作了个imx390dummypad,情况也是一样,中断没增加,也没有录到图像,media-ctrl -p看format没有什么不同了
sh fmt-dummy.sh
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -s 1920x1080 -f UYVY /dev/video2 -c100^C
root@am62axx-evm:/opt/edgeai-gst-apps# media-ctl -2023 Feb 27 10:38:50 am62axx-evm Process 1172 (edgeai-gui-app) of user 0 dumped core.
2023 Feb 27 10:38:50 am62axx-evm Process 1172 (edgeai-gui-app) of user 0 dumped core.
p
Media controller API version 5.10.168
Media device information
------------------------
driver j721e-csi2rx
model TI-CSI2RX
serial
bus info platform:30102000.ticsi2rx
hw revision 0x1
driver version 5.10.168
Device topology
- entity 1: 30102000.ticsi2rx (7 pads, 7 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "cdns_csi2rx.30101000.csi-bridge":1 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx context 0":0 [ENABLED,IMMUTABLE]
pad2: Source
-> "30102000.ticsi2rx context 1":0 [ENABLED,IMMUTABLE]
pad3: Source
-> "30102000.ticsi2rx context 2":0 [ENABLED,IMMUTABLE]
pad4: Source
-> "30102000.ticsi2rx context 3":0 [ENABLED,IMMUTABLE]
pad5: Source
-> "30102000.ticsi2rx context 4":0 [ENABLED,IMMUTABLE]
pad6: Source
-> "30102000.ticsi2rx context 5":0 [ENABLED,IMMUTABLE]
- entity 9: cdns_csi2rx.30101000.csi-bridge (5 pads, 2 links, 0 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: Sink
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "ds90ub960 4-003d":4 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "30102000.ticsi2rx":0 [ENABLED,IMMUTABLE]
pad2: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad3: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
pad4: Source
[stream:0 fmt:UYVY8_1X16/640x480 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
- entity 15: ds90ub960 4-003d (6 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev2
routes:
0/0 -> 4/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none]
<- "ds90ub953 4-0044":1 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none]
-> "cdns_csi2rx.30101000.csi-bridge":0 [ENABLED,IMMUTABLE]
pad5: Source
- entity 24: ds90ub953 4-0044 (2 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev3
routes:
0/0 -> 1/0 [ACTIVE]
pad0: Sink
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none colorspace:smpte170m]
<- "imx390dummy 6-001a":0 [ENABLED,IMMUTABLE]
pad1: Source
[stream:0 fmt:UYVY8_2X8/1920x1080 field:none colorspace:smpte170m]
-> "ds90ub960 4-003d":0 [ENABLED,IMMUTABLE]
- entity 29: imx390dummy 6-001a (1 pad, 1 link, 2 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev4
routes:
0/0 -> 0/0 [ACTIVE, IMMUTABLE, SOURCE]
0/0 -> 0/1 [INACTIVE, IMMUTABLE, SOURCE]
pad0: Source
[stream:0 fmt:UYVY8_2X8/1920x1080@1/30 field:none colorspace:smpte170m]
-> "ds90ub953 4-0044":0 [ENABLED,IMMUTABLE]
- entity 35: 30102000.ticsi2rx context 0 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video2
pad0: Sink
<- "30102000.ticsi2rx":1 [ENABLED,IMMUTABLE]
- entity 41: 30102000.ticsi2rx context 1 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video3
pad0: Sink
<- "30102000.ticsi2rx":2 [ENABLED,IMMUTABLE]
- entity 47: 30102000.ticsi2rx context 2 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video4
pad0: Sink
<- "30102000.ticsi2rx":3 [ENABLED,IMMUTABLE]
- entity 53: 30102000.ticsi2rx context 3 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video5
pad0: Sink
<- "30102000.ticsi2rx":4 [ENABLED,IMMUTABLE]
- entity 59: 30102000.ticsi2rx context 4 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video6
pad0: Sink
<- "30102000.ticsi2rx":5 [ENABLED,IMMUTABLE]
- entity 65: 30102000.ticsi2rx context 5 (1 pad, 1 link, 0 route)
type Node subtype V4L flags 0
device node name /dev/video7
pad0: Sink
<- "30102000.ticsi2rx":6 [ENABLED,IMMUTABLE]
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# yavta -s 1920x1080 -f UYVY /dev/video2 -c100
Device /dev/video2 opened.
[ 45.194119] zyk ti_csi2rx_queue_setup 823
Device `j721e-csi2rx' on `platform:30102000.ticsi2rx' is a video[ 45.202359] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 0, plane 0 offset 0x00000000
output (without mplanes) device.
Video format set: UYVY (59565[ 45.217124] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 1, plane 0 offset 0x003f5000
955) 1920x1080 (stride 3840) field none buffer size 4147200
Vid[ 45.232340] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 2, plane 0 offset 0x007ea000
eo format: UYVY (59565955) 1920x1080 (stride 3840) field none bu[ 45.247598] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 3, plane 0 offset 0x00bdf000
ffer size 4147200
[ 45.262464] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 4, plane 0 offset 0x00fd4000
[ 45.273497] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 5, plane 0 offset 0x013c9000
[ 45.284784] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 6, plane 0 offset 0x017be000
[ 45.296014] videobuf2_common: [cap-00000000cb995559] __setup_offsets: buffer 7, plane 0 offset 0x01bb3000
[ 45.305733] videobuf2_common: [cap-00000000cb995559] __vb2_queue_alloc: allocated 8 buffers, 1 plane(s) each
8 buffers requested.
[ 45.315896] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 0, plane 0 successfully mapped
length: 4147200 offset: 0 timestamp type/source: mono/EoF
[ 45.326905] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 1, plane 0 successfully mapped
Buffer 0/0 mapped at address 0xffff90858000.
length: 4147200 of[ 45.340994] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 2, plane 0 successfully mapped
fset: 4149248 timestamp type/source: mono/EoF
Buffer 1/0 mapped[ 45.355768] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 3, plane 0 successfully mapped
at address 0xffff90463000.
length: 4147200 offset: 8298496 tim[ 45.370292] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 4, plane 0 successfully mapped
estamp type/source: mono/EoF
Buffer 2/0 mapped at address 0xfff[ 45.385079] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 5, plane 0 successfully mapped
f9006e000.
length: 4147200 offset: 12447744 timestamp type/sour[ 45.399614] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 6, plane 0 successfully mapped
ce: mono/EoF
Buffer 3/0 mapped at address 0xffff8fc79000.
leng[ 45.414405] videobuf2_common: [cap-00000000cb995559] vb2_mmap: buffer 7, plane 0 successfully mapped
th: 4147200 offset: 16596992 timestamp type/source: mono/EoF
Bu[ 45.428887] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 0 succeeded
ffer 4/0 mapped at address 0xffff8f884000.
length: 4147200 offs[ 45.443092] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 1 succeeded
et: 20746240 timestamp type/source: mono/EoF
Buffer 5/0 mapped [ 45.457113] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 2 succeeded
at address 0xffff8f48f000.
length: 4147200 offset: 24895488 tim[ 45.471343] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 3 succeeded
estamp type/source: mono/EoF
Buffer 6/0 mapped at address 0xfff[ 45.485408] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 4 succeeded
f8f09a000.
length: 4147200 offset: 29044736 timestamp type/sour[ 45.485418] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 5 succeeded
ce: mono/EoF
Buffer 7/0 mapped at address 0xffff8eca5000.
[ 45.513652] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 6 succeeded
[ 45.513664] videobuf2_common: [cap-00000000cb995559] vb2_core_qbuf: qbuf of buffer 7 succeeded
[ 45.536178] zyk ti_csi2rx_buffer_queue 875
[ 45.540487] zyk ti_csi2rx_buffer_queue 875
[ 45.544616] zyk ti_csi2rx_buffer_queue 875
[ 45.544622] zyk ti_csi2rx_buffer_queue 875
[ 45.552954] zyk ti_csi2rx_buffer_queue 875
[ 45.552958] zyk ti_csi2rx_buffer_queue 875
[ 45.552961] zyk ti_csi2rx_buffer_queue 875
[ 45.552963] zyk ti_csi2rx_buffer_queue 875
[ 45.570942] zyk ti_csi2rx_start_dma 771
[ 45.574949] videobuf2_common: [cap-00000000cb995559] vb2_core_streamon: successful
[ 45.582596] videobuf2_common: [cap-00000000cb995559] __vb2_wait_for_done_vb: will sleep waiting for buffers
^Z[ 48.565869] videobuf2_common: [cap-00000000cb995559] __vb2_wait_for_done_vb: sleep was interrupted
[1]+ Stopped(SIGTSTP) yavta -s 1920x1080 -f UYVY /dev/video2 -c100
root@am62axx-evm:/opt/edgeai-gst-apps# sh C0.sh
953 config
953 end config
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps#
root@am62axx-evm:/opt/edgeai-gst-apps# fg
yavta -s 1920x1080 -f UYVY /dev/video2 -c100[ 54.197831] videobuf2_common: [cap-00000000cb995559] __vb2_wait_for_done_vb: will sleep waiting for buffers
网上查了一下,dump了一下寄存器

,CSI_RX_IF_VBUS2APB_STREAM0_STATUS 0x30101048 有2,3变化,说明dphy有数据,
但
CSI_RX_IF_VBUS2APB_ERROR_IRQS 0x30101028 显示bit 8置位

项目急啊,大哥哥
我们模组型号
SG2-OX03CC-5200-FPDLink
看他们官网,他们在你们平台上调试过的