Part Number: PROCESSOR-SDK-AM62A
Hi Ti
For AM62A Version: 09.01.00.39, I have some questions to consult you, as follows:
1 From the current code point of view, the baseline only updates Linux, what are the update points for openvx?
2 At present, I can view some code of openvx. Is openvx a node of Gstreamer as mentioned before?
3 In addition, the previous baseline drive development, if the migration to the latest baseline, can be directly transplanted, or need to be modified?
Thanks.