This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62A: AM62A Version: 09.01.00.39 Consultation on related questions

Part Number: PROCESSOR-SDK-AM62A


Hi Ti

For AM62A Version: 09.01.00.39, I have some questions to consult you, as follows:

1 From the current code point of view, the baseline only updates Linux, what are the update points for openvx?

2 At present, I can view some code of openvx. Is openvx a node of Gstreamer as mentioned before?

3 In addition, the previous baseline drive development, if the migration to the latest baseline, can be directly transplanted, or need to be modified?

Thanks.