HI TI:
我们在使用tda4vm 7.3sdk上面,当我同时运行vx_app_single_cam和另一个摄像头相关的进程,会出现i2c操作timeout的情况,因为两个进程有可能会同时去操作i2c,从而导致i2c操作异常,请问有解决方法吗
已知我们必须让两个进程这样来运行,不能调整其运行顺序
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI:
我们在使用tda4vm 7.3sdk上面,当我同时运行vx_app_single_cam和另一个摄像头相关的进程,会出现i2c操作timeout的情况,因为两个进程有可能会同时去操作i2c,从而导致i2c操作异常,请问有解决方法吗
已知我们必须让两个进程这样来运行,不能调整其运行顺序
请问有解决方法吗
1. 使用锁(Lock):在代码中使用锁机制,确保同一时间只有一个进程能够访问I2C总线。当一个进程在访问I2C时,其他进程必须等待锁的释放。
from multiprocessing import Lock # 在代码中定义锁 i2c_lock = Lock() # 在需要访问I2C的地方使用锁 with i2c_lock: # 执行I2C操作的代码
2. 用 IPC:用进程间通信机制,例如消息队列或共享内存,在进程之间共享I2C访问的状态信息。通过在共享数据上加锁,确保只有一个进程能够修改共享的I2C状态。
3. 分配独立的I2C总线:为每个进程分配独立的I2C总线。可以避免进程之间的冲突。
4. 调整I2C设备地址:每个进程中使用不同的I2C设备地址,从而避免冲突。
5. 选择支持多主机模式的I2C总线设备,或者使用I2C多路复用器来隔离不同进程的I2C访问。
您好,抱歉我目前没有找到参考,我通过个人理解为您写了一段示例代码框架,用互斥锁来保护多任务下的I2C访问,请参考。
// 假设I2C设备地址
#define I2C_DEVICE_ADDRESS 0x50
// 定义全局互斥锁
SemaphoreHandle_t i2cMutex;
// 模拟I2C读取函数
void simulated_i2c_read() {
// 模拟I2C读取操作
// ...
}
// 模拟I2C写入函数
void simulated_i2c_write() {
// 模拟I2C写入操作
// ...
}
// 1:读取I2C数据
void task_read_i2c(void *pvParameters) {
while (1) {
// 尝试获取I2C互斥锁
if (xSemaphoreTake(i2cMutex, portMAX_DELAY)) {
// 执行I2C读取操作
simulated_i2c_read();
// 释放I2C互斥锁
xSemaphoreGive(i2cMutex);
}
// 任务延时
vTaskDelay(pdMS_TO_TICKS(1000));
}
}
// 2:写入I2C数据
void task_write_i2c(void *pvParameters) {
while (1) {
// 尝试获取I2C互斥锁
if (xSemaphoreTake(i2cMutex, portMAX_DELAY)) {
// 执行I2C写入操作
simulated_i2c_write();
// 释放I2C互斥锁
xSemaphoreGive(i2cMutex);
}
// 任务延时
vTaskDelay(pdMS_TO_TICKS(500));
}
}
int main(void) {
// 初始化I2C互斥锁
i2cMutex = xSemaphoreCreateMutex();
// 创建任务
xTaskCreate(task_read_i2c, "ReadI2C", configMINIMAL_STACK_SIZE, NULL, tskIDLE_PRIORITY + 1, NULL);
xTaskCreate(task_write_i2c, "WriteI2C", configMINIMAL_STACK_SIZE, NULL, tskIDLE_PRIORITY + 1, NULL);
// 启动调度器
vTaskStartScheduler();
while (1) {
}
return 0;
}
如有问题欢迎您的指正,谢谢
你好,我的代码如下
错误打印如下:
[MCU2_0] 1604.296556 s: Error : I2C Timeout while writing: i2chandle[1]
[MCU2_0] 1604.296673 s: Error : I2C Timeout while writing: i2chandle[1]
[MCU2_0] 1604.296787 s: Error : I2C Timeout while writing: i2chandle[1]
[MCU2_0] 1604.296901 s: Error : I2C Timeout while writing: i2chandle[1]
看起来是I2C总线上有问题。你可以排查一下:硬件连接、I2C配置、I2C设备状态、中断
再者:I2C API返回值的错误处理。我看你检查了`status`是否为0,但你还要需要查看一下具体的错误代码
最后:在调试时,你可以尝试先简化你的代码,只保留最基本I2C访问,确保在最简单的情况下没有超时问题。然后逐步添加其他功能