This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62A: Processor sdk Linux for AM62Ax build problem

Part Number: PROCESSOR-SDK-AM62A

Hi export,

我按照以下步骤下载编译Processor sdk Linux for AM62Ax,但是yocto编译出错,无法继续。请帮忙检查一下是什么问题。

参考文档software-dl.ti.com/.../Overview_Building_the_SDK.html

1)./ti_cgt_armllvm_3.2.0.LTS_linux-x64_installer.bin
2) cd ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/
./setup.sh
3)cd yocto-build/
./oe-layertool-setup.sh -f configs/processor-sdk-analytics/processor-sdk-analytics-09_01_00-config.txt
cd build
./conf/setenv
echo 'ARAGO_BRAND = "edgeai"' >> conf/local.conf
MACHINE=am62axx-evm bitbake -k tisdk-edgeai-image
Error log:
igs@igs:build$ MACHINE=am62axx-evm bitbake -k tisdk-edgeai-image
/usr/lib/python3/dist-packages/html5lib/_trie/_base.py:3: DeprecationWarning: Using or importing the ABCs from 'collections' instead of from 'collections.abc' is deprecated since Python 3.3, and in 3.10 it will stop working
  from collections import Mapping
NOTE: Your conf/bblayers.conf has been automatically updated.
NOTE: Your conf/bblayers.conf has been automatically updated.
NOTE: Started PRServer with DBfile: /home/igs/data/AM62/ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/yocto-build/build/cache/prserv.sqlite3, Address: 127.0.0.1:42813, PID: 17747
ERROR: Directory name ${OEBASE}/build/sstate-cache contains unexpanded bitbake variable. This may cause build failures and WORKDIR polution.
  • 看报错似乎是yocto的python程序执行失败,能否确认一下咱用的ubuntu系统,是否和原文档要求的是一个版本,以及有没有动过里面的比如python的版本

  • 我的是ubuntu20.04,修改了修改bin/setup-host-check.sh文件适配自己的版本。修改如下:

    get_host_type host

    #if [ "$host" != "jammy" ]; then
    # echo "Unsupported host Linux $host. Only Ubuntu 22.04 LTS is supported"
    # exit 1
    #fi
    if [ "$host" != "focal" ]; then
    echo "Unsupported host Linux $host. Only Ubuntu 20.04 LTS is supported"
    exit 1
    fi

    python3安装的版本为3.8,必须用3.10吗?

    igs@igs:mcu_plus_sdk_am62ax_09_01_00_39$ python3 --version
    Python 3.8.10

  • 我看你发的文档链接:https://software-dl.ti.com/processor-sdk-linux/esd/AM62AX/09_01_00/exports/docs/linux/Overview_Building_the_SDK.html

    要求是ubuntu 22.04

    那你用22.04就是最容易编译成功的,也是TI测试过的

    用其他版本并不是说不行,但肯定会有各种问题需要解决,除了yocto自身的(python版本问题),还有后面构建系统时会遇到各种奇奇怪怪的问题