Part Number: SK-AM68
Hi, Experts:
I bought SK-AM68 and tried demo of "Edge AI gallery".
I noticed the left side function of "Custom". The function is able to select Input type, Image and Model with GUI.
How to execute ONR-OD-xxx or TVM-OD-xxx from the command line?
In the case, is able to return resoult by file ?
Or, is there any API able to call for this?
By the way, I want to let SK-AM68 as a co-processor for object detection.
I think that is the easy/simple/lazy/fastest way to test/demo/apply/deploy TI AI solution.
Using gigaLAN/TCP input JPG and output/return result by XML/JSON/text.
If I finish this I will publish the code to gitHub.
Best Regards,
Greatcat