This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Linux userspace RPMsg example 下载不了

Part Number: AM625


Building the Linux userspace RPMsg example#

Note

These steps were tested on Ubuntu 18.04. Later versions of Ubuntu may need different steps.

Access source code in the git repo here. rproc_id is defined at include/rproc_id.h.

Build the Linux Userspace example for Linux RPMsg by following the steps in the top-level README:

  1. Download the git repo

  2. Install GNU autoconf, GNU automake, GNU libtool, and v8 compiler as per the README

  3. Perform the Build Steps as per the README

    请提供有效下载方法。