This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: 为保证DDR和EMMC在突然掉电时,有足够的时间来进行保存数据,避免数据调和器件损坏,系统电源监控引脚VMON_VSYS应该怎么处理?

Part Number: AM623

本设计采用使用24V转5V ,然后5V给PMIC供电。为保证DDR4和EMMC在突然掉电时,有足够的时间来进行保存数据,避免数据调和器件损坏,就需要对电源电路更加电解电容来延缓系统的掉电时间,来确保DDR等器件能正常保存数据。现在想到的办法有两种:

  1. 在24V端加电容,系统电源监控引脚VMON_VSYS接在5V端,24V掉电时,5V不会立即掉电,但是VMON_VSYS检测不到系统出现了掉电情况知道5V的电也掉下去为止(DEMO板是这样处理的),我认为无法起到保护数据的作用
  2. 在5V端加电容,系统电源监控引脚VMON_VSYS接在24V,24V掉电时,VMON_VSYS会立即检测到系统出现了掉电情况,由于5V这端增加了电容不会立即掉电,从而起到延长AM62处理器掉电的时间,进而起到保护数据的作用

我个人更倾向于第二种方案,但是24电压过高,同时VMON_VSYS的电压检测范围过窄,直接将VMON_VSYS接到24V,请问这种做法是否可行?会不会有很大的风险,麻烦给出一些合理的建议,谢谢!!!

  • 建议到电源论坛咨询。
    https://e2echina.ti.com/support/power-management/f/power-management-forum

    另外,可以先参考下面的文档。
    VMON_VSYS (Recommend provisioning the external resistor voltage divider for early supply failure indication irrespective of the software implementation). For connecting the system voltage (main supply voltage such as 3.3 V, 5 V or other voltage levels) through an external resistor voltage divider, see the System Power Supply Monitor Design Guidelines section of the device-specific data sheet. It is recommend to implement a noise filter (capacitor) across the voltage divider output since VMON_VSYS has minimum hysteresis and a high-bandwidth response to transients.
    https://www.ti.com/lit/an/sprad05b/sprad05b.pdf