Part Number: AM623
本设计采用使用24V转5V ,然后5V给PMIC供电。为保证DDR4和EMMC在突然掉电时,有足够的时间来进行保存数据,避免数据调和器件损坏,就需要对电源电路更加电解电容来延缓系统的掉电时间,来确保DDR等器件能正常保存数据。现在想到的办法有两种:
- 在24V端加电容,系统电源监控引脚VMON_VSYS接在5V端,24V掉电时,5V不会立即掉电,但是VMON_VSYS检测不到系统出现了掉电情况知道5V的电也掉下去为止(DEMO板是这样处理的),我认为无法起到保护数据的作用
- 在5V端加电容,系统电源监控引脚VMON_VSYS接在24V端,24V掉电时,VMON_VSYS会立即检测到系统出现了掉电情况,由于5V这端增加了电容不会立即掉电,从而起到延长AM62处理器掉电的时间,进而起到保护数据的作用
我个人更倾向于第二种方案,但是24电压过高,同时VMON_VSYS的电压检测范围过窄,直接将VMON_VSYS接到24V,请问这种做法是否可行?会不会有很大的风险,麻烦给出一些合理的建议,谢谢!!!