Part Number: PROCESSOR-SDK-J721E
Question 1: Can the XDS100V2 debugger be used to debug the J721EXSKG01EVM? There is an interface mismatch between them; the XDS100V2 has a 14-pin interface, while the JTAG interface on the J721EXSKG01EVM is 20 pins. Is it that only the XDS110, XDS200, and XDS560v2 debuggers can be used?
Question 2: How can I burn a program written in CCS onto the J721E without using a debugger?