This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: 中断嵌套问题

Part Number: TMS320C6678

需求如下:

DSP同时使用SRIO中断及UART中断(本项目仅使用单核,不考虑多核),目前遇到的问题如下:

 

网上找到的例程,都是针对单种外设进行CIC配置,我单独配置SRIO中断或者UART中断,都能正常,但如果两种外设都要使用,且使用中断,就会出现无法同时使用的情况,经过多次排查,感觉还是中断配置的地方有问题,疑问之处已经用黄底标出,请帮看下!具体代码段如下:

 

CSL_CPINTC_Handle hnd; //两种中断需要创建2个Handle吗?

CSL_IntcContext intcContext;

CSL_IntcEventHandlerRecord EventHandler[30];//里面是用到几个中断就有几个EventHandler子元素?

CSL_IntcGlobalEnableState state;//多种中断能否共用?

CSL_IntcEventHandlerRecord EventRecord;

//SRIO读数

CSL_IntcObj intcObj_read;

CSL_IntcHandle read_handle;

CSL_IntcParam vectId_read;

//UART

CSL_IntcObj intcObj_uart;

CSL_IntcHandle uart_handle;

CSL_IntcParam vectId_uart;

uint8_t eventId_uart;

 

#define host_event 2//SRIO主机中断

#define sys_event  CSL_INTC0_INTDST0//0x70

 

    /************************************************

     *************** INTC Configuration *************

     ************************************************/

 

    /* INTC module initialization */

    intcContext.eventhandlerRecord = EventHandler;    intcContext.numEvtEntries = 2;  //此处为1不行,如果改成1的话连单个中断都不能用,请问是什么原因?

    if (CSL_intcInit(&intcContext) != CSL_SOK) {

        return -1;

    }

 

    /* Enable NMIs */

    if (CSL_intcGlobalNmiEnable() != CSL_SOK) {

        return -1;

    }

 

    /* Enable global interrupts */

    if (CSL_intcGlobalEnable(&state) != CSL_SOK) {

        return -1;

    }

 

    /**************************************************

     ************* CPINTC-0 Configuration *************

     **************************************************/

    /* Open the handle to the CPINT Instance */

    hnd = CSL_CPINTC_open(0);

//此处为0,如果要配两种中断,是否需要再单独创建hnd1 = CSL_CPINTC_open(0) or CSL_CPINTC_open(1)??

    if (hnd == 0) {

        return -1;

    }

 

    /* Disable all host interrupts. */

    CSL_CPINTC_disableAllHostInterrupt(hnd);

 

    /* Configure no nesting support in the CPINTC Module. */

    CSL_CPINTC_setNestingMode(hnd, CPINTC_NO_NESTING);

 

 

    /* We now map System Interrupt INTDST0 to channel 2 */

    CSL_CPINTC_mapSystemIntrToChannel(hnd, sys_event, host_event);   //CIC0 Event Inputs:RapidIO interrupt INTDST0

 

    //uart

    /*

     * Map system interrupt to channel

     * channel: CIC0_OUT(8+20*n) (n is core num) = 8

     */

    CSL_CPINTC_mapSystemIntrToChannel(hnd, CSL_INTC0_UARTINT, 8);

 

   

    CSL_CPINTC_clearSysInterrupt(hnd, CSL_INTC0_UARTINT);

 

    /* We now enable system interrupt  */

    CSL_CPINTC_enableSysInterrupt(hnd, sys_event);

    //uart

    CSL_CPINTC_enableSysInterrupt(hnd, CSL_INTC0_UARTINT);

 

    /* We enable host interrupts. */

    CSL_CPINTC_enableHostInterrupt(hnd, host_event);

    //uart

    CSL_CPINTC_enableHostInterrupt(hnd, 8);

 

    /* Enable all host interrupts also. */

    CSL_CPINTC_enableAllHostInterrupt(hnd);

 

    /* clear system interrupt  */

  CSL_CPINTC_clearSysInterrupt(hnd,sys_event);//CSL_INTC0_INTDST0:0x00000070

 

    vectId_read = CSL_INTC_VECTID_4;// CPU interrupt number

    read_handle = CSL_intcOpen(&intcObj_read, 62, &vectId_read, NULL);//62-CIC0_OUT(2),

 

 

    /* Open INTC, event ID 30/104 maps to CPU interrupt vector 13 */

    vectId_uart = CSL_INTC_VECTID_13;

uart_handle = CSL_intcOpen(&intcObj_uart, CSL_GEM_INTC0_OUT8_OR_INTC1_OUT8, &vectId_uart, NULL);

   if(uart_handle == NULL) {

        //uart_printf("Open intc_uart failed!\n");

        return -1;

    }

 

    //INTSEL7-4,11-8,15-12

    if (read_handle == NULL) {

        return -1;

    }

 

    if (uart_handle == NULL) {

        return -1;

    }

 

//不太能理解的是,多中断配置,是要先配一种,还是两种并行去配?下面这句绑定的最为可疑,标黄的地方如果是1,甚至会直接覆盖[0]的配置

    /* 这里将中断服务函数和中断源联系起来 */

    /* Bind ISR to Interrupt */

    EventHandler[0].handler = (CSL_IntcEventHandler) &read_isr_handler;

    EventHandler[0].arg = (void *)0;

 

    EventHandler[2].handler = (CSL_IntcEventHandler) &uart_isr;

    EventHandler[2].arg = (void *)CSL_INTC0_UARTINT;

 

    if (CSL_intcPlugEventHandler(read_handle, &EventHandler[0]) != CSL_SOK) {

        return -1;

    }

 

    if (CSL_intcPlugEventHandler(uart_handle, &EventHandler[2]) != CSL_SOK) {

        return -1;

    }

 

    /* clean event */

    CSL_intcHwControl(read_handle, CSL_INTC_CMD_EVTCLEAR, NULL);

    CSL_intcHwControl(uart_handle, CSL_INTC_CMD_EVTCLEAR, NULL);

 

    /* 使能刚才配置的两种中断通路 /

     / Enabling the read events. */

    if (CSL_intcHwControl(read_handle, CSL_INTC_CMD_EVTENABLE, NULL) != CSL_SOK) {

        return -1;

    }

   

    if (CSL_intcHwControl(uart_handle, CSL_INTC_CMD_EVTENABLE, NULL) != CSL_SOK) {

        return -1;

    }