This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: TI DEMO板:TMDS64EVM,原理图:PROC101D中3.3V,CPU电流设计为1A与使用TI功耗评估xls工具评估出的100mA相差巨大问题

Part Number: AM6442
Other Parts Discussed in Thread: TMDS64EVM, SK-AM64B

下图是TI的demo板TMDS64EVM,原理图:PROC101D中CPU的3.3V电流用电需求:1A

下图是使用TI 的功耗评估工具,各模块都按照较大利用里评估出的电流,3.3V只使用了不到100mA,与实际设计的1A相差巨大。

而另一个TI的demo评估板SK demo:SK-AM64B,对应原理图:PROC100 001 SKAM64,给CPU的3V3只留出了250mA(3A-400mA-200mA-100mA-500mA-500mA-1A-50mA=250mA),这个就与功耗评估工具的数据差不多。

所以我设计到底按照多少?按照实际功耗评估表的200mA左右设计还是按照1A设计?