最近调一个C6455的板子,在CCS4..2.4下遇到仿真器不能连接DSP的问题,总是跳出下面的提示:
Error connecting to the target:
(Error -1143 @ 0x0)
Device core was stalled, and recovery was successful.
Retry后,出现:
Error connecting to the target:
(Error -1202 @ 0xB000001C)
Device pipeline is 'not ready‘.
用的SEED XDS560PLUS的仿真器,另一块一样的板子连接就没有问题。
我也查了,8分频的时钟输出有,复位状态指示有,核电压,都正常。
请问各位专家这可能是哪儿的问题?需要从哪儿下手解决。是DSP焊接不好?还是DSP损坏?还是其他问题?