This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

仿真器连不上C6455 DSP



最近调一个C6455的板子,在CCS4..2.4下遇到仿真器不能连接DSP的问题,总是跳出下面的提示:

Error connecting to the target:
(Error -1143 @ 0x0)
Device core was stalled, and recovery was successful.

Retry后,出现:

Error connecting to the target:
(Error -1202 @ 0xB000001C)
Device pipeline is 'not ready‘.

用的SEED XDS560PLUS的仿真器,另一块一样的板子连接就没有问题。

我也查了,8分频的时钟输出有,复位状态指示有,核电压,都正常。

请问各位专家这可能是哪儿的问题?需要从哪儿下手解决。是DSP焊接不好?还是DSP损坏?还是其他问题?

  • JTAG口信号正常么?

  • 1.244芯片工作正常

    2.DSP CLK初始时钟约为500KHz,CONNECT过程中有波形变化,最后时钟为10.368M,示波器测试

    3.DSP TDI 初始电平H   CONNECT过程中有波形变化,示波器测试

    4.DSP TDO初始电平L  CONNECT过程中有波形变化,有输出,示波器测试

    5.DSP TMS初始电平 H   CONNECT过程中有波形变化,似数据,报错后,电平L

    6.EMU0初始电平 H  CONNECT过程中无波形变化,报错后,电平H

    7.EMU1 初始电平H  CONNECT过程中无波形变化,报错后,电平H

    8.DSP TRST 初始电平 L CONNECT过中程变H

  • 在CCS5下测了test connection,JTAG链正常。

    重新检查了配置,是AEA地址配置线上一个上拉电阻没有焊好。

    粗心大意害死人啊!