This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BT656时钟

Other Parts Discussed in Thread: TVP5147

请问如果使用BT656传输视频流时,L138使用VPIF接口接收该视频流,时钟必须为27M吗?24M可以吗?

  • 1. 对于输入,VP的位时钟是由外部提供。

    2. 对于输出,VP的位时钟可以由VP_CLKIN2/3提供,可以不从PLL分频过来。

  • Dear Tang:

         首先感谢您的回复!

         可能您误会我的意思了,我知道对于输入,VP的位时钟是由外部提供。我的意思是:当外部使用BT656格式传输视频流时,L138也配置为BT656捕获,外部提供给L138 VPIF接口的时钟必须为27M吗?24M是否可以?

  • PCLk是由外部信号决定的的,多少都可以。就看外部视频信号是否是标准的。

  • 现在外部视频信号是标准的BT656格式,你的意思是如果L138 channel0 配置为bt65捕获模式,CLKIN0为多少都可以吗?也就是CLKIN0不为27M也可以,是吗?

  • 如果外部提供的是标准的BT656 D1的信号,如果是480i, 576i,时钟为13.5MHz, 如果是480P, 576P,时钟为27MHz,怎么会出现24MHz呢?

    如果不是标准的,时钟为多少都可以,BT656的信号是内嵌同步,接口根据同步信号接收有效数据。

    你就把它当成一个数据接口,时钟高,速度就高,时钟低,速度就低。

  • 哦,感激您的回答,我们的硬件电路是这样连接的:L138 VPIF接口与CMOS ov7725相连,由于L138 EVM板上L138 VPIF接口是与TVP5147相连,而且EVM内核代码中将L138接口配置为BT656格式捕获模式,为了使用你们提供的驱动代码,我只修改了TVP514X.C中相关代码,使之能配置CMOS,能正常工作。但是网上给出的CMOS配置都是在时钟为24M的条件下配置寄存器的,如果现在改为27Mhz,帧速率肯定也不是25fps了(内核代码中默认的帧速率为25fps),是多少也不知道,也没有计算公式,所以我就想问一下,我们应该怎样配置CMOS才能与L138 VPIF接口匹配?或者说EVM 上tvp5147是怎么配置的?vp5147用的是标准的BT656吗?它的PCLK为多少?帧速率为多少?

  • 你说的:“如果外部提供的是标准的BT656 D1的信号,如果是480i, 576i,时钟为13.5MHz, 如果是480P, 576P,时钟为27MHz”中BT656 D1,480i, 576i,480P, 576P是什么意思啊?能解释一下吗?期待您的回复,谢谢!

  • Can anybody help me?