请问如果使用BT656传输视频流时,L138使用VPIF接口接收该视频流,时钟必须为27M吗?24M可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
哦,感激您的回答,我们的硬件电路是这样连接的:L138 VPIF接口与CMOS ov7725相连,由于L138 EVM板上L138 VPIF接口是与TVP5147相连,而且EVM内核代码中将L138接口配置为BT656格式捕获模式,为了使用你们提供的驱动代码,我只修改了TVP514X.C中相关代码,使之能配置CMOS,能正常工作。但是网上给出的CMOS配置都是在时钟为24M的条件下配置寄存器的,如果现在改为27Mhz,帧速率肯定也不是25fps了(内核代码中默认的帧速率为25fps),是多少也不知道,也没有计算公式,所以我就想问一下,我们应该怎样配置CMOS才能与L138 VPIF接口匹配?或者说EVM 上tvp5147是怎么配置的?vp5147用的是标准的BT656吗?它的PCLK为多少?帧速率为多少?