Part Number: AM3352
The TI SDK I used is: ti-processor-sdk-linux-am335x-evm-08.02.00.24 (download from TI web).
Uboot source code is: u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8 (include in the SDK above/board-support/)
Corss Compile is: arm-none-linux-gnueabihf- gcc (include in the SDK above/linux-devkit/sysroots/x86_64-arago-linux/usr/bin)
When I build the U-boot with original "am335x_evm_defconfig", the build is sucessfully,
After I follow the insturctions "software-dl.ti.com/.../U-Boot.html" step to step to set baseline of my own design board, I build the U-boot as follow, but found error:
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' mrproper —— this is O.K.
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' am335x_<myboard>_defconfig ——.config is generated sucessfully.
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' ——error
/opt/ti-processor-sdk-linux-am335x-evm-08.02.00.24/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/am335x_dcx11_3/../common/image-fdt.c:575: undefined reference to `ft_board_setup'
arm-none-linux-gnueabihf-ld.bfd: common/built-in.o:(.data.init_sequence_r+0x2c): undefined reference to `board_init'
arm-none-linux-gnueabihf-ld.bfd: common/built-in.o:(.data.init_sequence_r+0x94): undefined reference to `board_late_init'
/opt/ti-processor-sdk-linux-am335x-evm-08.02.00.24/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/Makefile:1762: recipe for target 'u-boot' failed
make[1]: *** [u-boot] Error 1
make[1]: Leaving directory '/opt/ti-processor-sdk-linux-am335x-evm-08.02.00.24/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/am335x_dcx11_3'
Makefile:167: recipe for target 'sub-make' failed
make: *** [sub-make] Error 2
Could you please help to check why this error occurs and how to deal with it?
Thnaks.