This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TI SDK I used is: ti-processor-sdk-linux-am335x-evm-08.02.00.24 (download from TI web).
Uboot source code is: u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8 (include in the SDK above/board-support/)
Corss Compile is: arm-none-linux-gnueabihf- gcc (include in the SDK above/linux-devkit/sysroots/x86_64-arago-linux/usr/bin)
When I build the U-boot with original "am335x_evm_defconfig", the build is sucessfully,
After I follow the insturctions "software-dl.ti.com/.../U-Boot.html" step to step to set baseline of my own design board, I build the U-boot as follow, but found error:
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' mrproper —— this is O.K.
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' am335x_<myboard>_defconfig ——.config is generated sucessfully.
make ARCH=arm CROSS_COMPILE='arm-none-linux-gnueabihf-' ——error
/opt/ti-processor-sdk-linux-am335x-evm-08.02.00.24/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/am335x_dcx11_3/../common/image-fdt.c:575: undefined reference to `ft_board_setup'
arm-none-linux-gnueabihf-ld.bfd: common/built-in.o:(.data.init_sequence_r+0x2c): undefined reference to `board_init'
arm-none-linux-gnueabihf-ld.bfd: common/built-in.o:(.data.init_sequence_r+0x94): undefined reference to `board_late_init'
/opt/ti-processor-sdk-linux-am335x-evm-08.02.00.24/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/Makefile:1762: recipe for target 'u-boot' failed
make[1]: *** [u-boot] Error 1
make[1]: Leaving directory '/opt/ti-processor-sdk-linux-am335x-evm-08.02.00.24/board-support/u-boot-2021.01+gitAUTOINC+44a87e3ab8-g44a87e3ab8/am335x_dcx11_3'
Makefile:167: recipe for target 'sub-make' failed
make: *** [sub-make] Error 2
Could you please help to check why this error occurs and how to deal with it?
Thnaks.
Hi kai,
For your query, please post your query in E2E Forum as link below.
https://e2e.ti.com/
TI's product line experts will answer your question.