This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于AM3359 GPMC异步通信问题



首先介绍一下硬件板设计情况,GPMC片选使用了两个,CS0连接norFlash,CS1连接fpga

在和FPGA进行通信的过程中为了提高速度,使用示波器对时序进行抓取进行分析,发现有这样一个问题:在对读写总周期,及片选时序进行调整时,连续两次访问片选之间的时间(nCS高电平持续时间)总是不变,有210ns,因为这个时间大小不变导致在传输20KB数据时, 用时2.8ms。尝试调制各种参数值都不能降低210ns这个时间。

我的时序设置是这样的:

#define  GPMC_CS1_CONFIG1    0x00001010

#define  GPMC_CS1_CONFIG2    0x00060600

#define  GPMC_CS1_CONFIG3    0x00020201

#define  GPMC_CS1_CONFIG4    0x02020202

#define  GPMC_CS1_CONFIG5    0x00060606

#define  GPMC_CS1_CONFIG6    0x03030000

#define  GPMC_CS1_CONFIG7    0x00000f04

不知道各位在使用过程中有没有遇到这样的问题。或者在相似的总线设置下(异步,16位)数据传输速度能达到多少?

谢谢!