This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 问题请教



1EMIF16每个CE空间可以连接多大容量的SRAM/NOR FLASH?是按照地址线去计算的吗,32MBNAND FLASH是支持一个CE空间64MB还是256MB
2)通过EMIF16NOR FLASH进行BOOT时,支持的是8bit还是16bit总线,手册中并没有明确说明。
3DDR3的参考时钟外接50MHz时,可以工作于DDR3-800DDR3-1066DDR3-1333DDR3-1600吗?如果不行,那么多少MHz的时钟可以支持这四种速率?