This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6614 算出来的cvdd核电压偏低,dsp核在跑业务时挂掉。

Other Parts Discussed in Thread: TPS56121, LM10011

焊接了一批板子,发现CVDD差别很大,从0.934V到1.02V都有。  

 其中0.934V核电压的板子,DSP核在跑业务时会挂掉。

电源芯片选的是TPS56121+LM10011 方案。  量了DSP出来的6bit调压数据是 011010 对应 0.866V。

我去掉LM10011输出电流串阻,CVDD为1.105V左右,此时,DSP核不会挂,显然,DSP挂的原因是因为cvdd过低的原因。

两个问题:

1. 同一批DSP的CVDD出来的调压差别这么大是否正常?  出来0.866V的调压要求是否正常?

2. CVDD电压可调是否仅仅是为功耗考虑,如果不好解决这个一致性问题,我去掉调压功能,将CVDD固定在1.1V左右,是否OK?