使用am335x做的板子,之前因为上电错误,335x的3.3V对地短路了,现在更换CPU后,板子大部分功能正常,但是引出的一个TTL的串口和一个RS485接口无法打开,测量串口和RS485对地、对核心板的3.3V阻抗均未发现明显的短路或断路情况,请问可能是什么原因呢?CPU虚焊?PS:调试串口工作正常。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用am335x做的板子,之前因为上电错误,335x的3.3V对地短路了,现在更换CPU后,板子大部分功能正常,但是引出的一个TTL的串口和一个RS485接口无法打开,测量串口和RS485对地、对核心板的3.3V阻抗均未发现明显的短路或断路情况,请问可能是什么原因呢?CPU虚焊?PS:调试串口工作正常。
建议你先核查一下上电时序,确认你的板子是否正常启动了,如果设置了UART0启动,至少串口应该会打印CCCC,如果没有cccc输出,说明上电有问题,芯片还是没起来。
板子已经正常启动了,调试串口为UART0,可以输出打印信息,板子上的其他功能,比如网络、音频、USB等都可正常工作,只有UART1和UART2,想要测试串口通信,输入命令后,打印信息显示无法打开。
检查下UART1和UART2的pinmux功能有没有设对