This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: SRIO 收发问题

Part Number: TMS320C6678


各位专家好,现在通过FPGA给C6678进行SRIO数据发送,采用的是SWRITE模式,传输的数据是图像数据。每发一帧图像,再发一个门铃信号。1秒50fps

现在实测,发送1700~2000包数据/门铃后,SRIO就卡死了不发,但是LINK状态还在。

试着降速到1.25GBPS现象还是存在。

试着降低门铃的发送频率,原来是1秒50个门铃,现在改成1秒5个,依然是DSP收到1700`2000个门铃后卡死。

158寄存器,显示的是遇到了包重传,无法进行下一次操作。

请问大概是哪方面原因。