This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14的5 Port Ethernet SWITCH能否实现诸如Broadcom BCM5389那样的交换性能?

Other Parts Discussed in Thread: 66AK2H14

以往的产品设计中,比如单板卡上可能有3个DSP、2个FPGA,希望通过SGMII互联,然后选用BCM5389这样的以太网SWITCH把3个DSP和2个FPGA互联,如图1

但是如今66AK2H14支持4个SGMII口,如果我单板要实现1片66AK2H14+2片C6678+2片FPGA,这样的话,我将2片C6678和2片FPGA连接到66AK2H14上,如图2

比较上述两图,图2能否达到图1那样的两两以太网交换的性能?或者说用66AK2H14内部的以太网SIWTCH替代BCM5389,会有哪些优势、劣势?

  • 可以做到,需要对K2H内部ALE进行路由配置,对不同的包进行数据路由分发。但是这样的话6678、FPGA之间的网络数据传递都需要走一遍66AK2H14内部的switch。

  • 嗯,我理解。

    图1中C6678和FPGA都要走一遍BCM5389,图2中C6678和FPGA都要走一边66AK2H14内部的Switch,这两者方式比较性能的话,会有很大差别吗?比如图2方式会明显弱于图1?

    如果两者性能差不多,就是说66AK2H14内部的Switch与BCM5389的throughput、latency都差不多,在做板时,我就可以完全省去一块BCM5389芯片了。