Other Parts Discussed in Thread: TMS320C6678
开发环境:windows32 CCS5.5
仿真器: WintechDigital XDS560V2 STM USB Emulator
硬件:自制C6678开发板
在新建的Target Configuration的Basic->connection选择WintechDigital XDS560V2 STM USB Emulator_0,Basic->Device选择TMS320C6678,然后在Advanced里给core0添加evmc6678l.gel,保存后点击TestConnection,然后出现如下信息:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\asus\AppData\Local\.TI\1592892923\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
Loaded FPGA Image: E:\CCS_V5\ccsv5\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Aug 19 2013'.
The library build time was '22:41:20'.
The library package version is '5.1.229.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the Nano-TBC VHDL.
The link is a 560-class second-generation-560 cable.
The software is configured for Nano-TBC VHDL features.
The controller will be software reset via its registers.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The controller will use falling-edge timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '2' (0x0002).
The utility logic has not previously detected a power-loss.
The utility logic is not currently detecting a power-loss.
Loaded FPGA Image: E:\CCS_V5\ccsv5\ccs_base\common\uscif\dtc_top.jbc
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-501' (0xfffffe0b).
The title is 'SC_ERR_TEST_MEASURE'.
The explanation is:
The built-in scan-path length measurement failed.
The built-in scan-path reliability tests cannot be performed without knowledge of the scan-path length. Try specifying the scan-path lengths in the command-line options or board configuration file of this utility or debugger.
[End]
因为仿真器是刚买的,自制开发板还是第一次连接仿真器,所以硬件和仿真器驱动可能都会有问题,但C6678的上电应该是没有问题的,板子的DSP原理图是参考EVM6678的,前期检测到设置boot mode的GPIO电平有问题,但应该不影响仿真器连接吧,驱动的安装一开始是有问题的,后来卸了重装开起来是正常的,现在也没有其他仿真器或者完好的板子用来验证排除问题,想请教下通过以上的原因能不能锁定其中一种(软件驱动或硬件问题),硬件要检测那些?