This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: TI-Processor-SDK-0802的U-boot问题

Part Number: AM3352


专家您好!

我们之前使用的SDK版本为ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install.bin,现在必须要进行升级,

前段时间ti-processor-sdk-linux-am335x-evm-09.01.00.001-Linux-x86-Install.bin,编译的时候有问题未解决。

现在使用ti-processor-sdk-linux-am335x-evm-08.02.00.24-Linux-x86-Install.bin移植通过后,

将MLO、u-boot.img、zImage、am335x-evm.dtb拷贝到boot文件夹下执行,出现找不到SD的错,显示信息如下。

U-Boot 2021.01-00001-gc59bf25a38-dirty (Dec 25 2024 - 10:22:43 +0800)

CPU  : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM:  512 MiB
WDT:   Started with servicing (60s timeout)
NAND:  0 MiB
MMC:   OMAP SD/MMC: 0
Loading Environment from FAT... <ethaddr> not set. Validating first E-fuse MAC
Net:   Could not get PHY for ethernet@4a100000: addr 0
eth2: ethernet@4a100000, eth3: usb_ether
Hit any key to stop autoboot:  0
MMC Device 1 not found
no mmc device at slot 1

之前ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install.bin的都能正常运行,还请专家能够指点一下!

非常感谢!

秦龙