Part Number: AM3352
专家您好!
我们之前使用的SDK版本为ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install.bin,现在必须要进行升级,
前段时间ti-processor-sdk-linux-am335x-evm-09.01.00.001-Linux-x86-Install.bin,编译的时候有问题未解决。
现在使用ti-processor-sdk-linux-am335x-evm-08.02.00.24-Linux-x86-Install.bin移植通过后,
将MLO、u-boot.img、zImage、am335x-evm.dtb拷贝到boot文件夹下执行,出现找不到SD的错,显示信息如下。
U-Boot 2021.01-00001-gc59bf25a38-dirty (Dec 25 2024 - 10:22:43 +0800)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 512 MiB
WDT: Started with servicing (60s timeout)
NAND: 0 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... <ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for ethernet@4a100000: addr 0
eth2: ethernet@4a100000, eth3: usb_ether
Hit any key to stop autoboot: 0
MMC Device 1 not found
no mmc device at slot 1
之前ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install.bin的都能正常运行,还请专家能够指点一下!
非常感谢!
秦龙