Part Number: SK-AM62A-LP
基于SK-AM62A-LP E3开发板,通过HDMI接口,如何点不同分辨率的屏幕?如何更改时钟,是否可以点8bit/10bit,有没有参考资料?
以上问题,期待您的回复,非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SK-AM62A-LP
基于SK-AM62A-LP E3开发板,通过HDMI接口,如何点不同分辨率的屏幕?如何更改时钟,是否可以点8bit/10bit,有没有参考资料?
以上问题,期待您的回复,非常感谢!
您好,我想知道SK-AM62A-LP支持的HDMI的限制是多少?
我需要点类似于如下几个非标准分辨率
8inch 1350x810@60hz pixel clock frequency=84.25Mhz 8bit
11inch 2000x810@60Hz pixel clock frequency=117.180Mhz 8bit/10bit
17.7inch 3400x1300@60Hz pixel clock frequency=283.5Mhz 8bit/10bit
点亮方式
1.不读取edid,HDMI强制输出;或者uboot启动时设置,直接可以输出?
2.读取edid,通过读到的edid,设置对应的HDMI时序,
以上问题,请帮忙看看,推荐些资料,非常感谢!
为了达到预期,我们在AM62A上不支持HDMI。我们通过SII9022A电桥将DPI信号转换为HDMI。我相信这座桥只支持最高1920x1080分辨率。这与TI SOC无关,而是与桥接限制有关。我们的最大PCLK为165MHz,因此我们可以支持高达该PCLK的分辨率。您上面列出的分辨率不是我们测试过的,我们的EVM+SW仅在1920x1080分辨率下进行了测试。
您好,
如果我这边点最大不超过1920x1080和PCLK=165MHz的通过DPI转换为HDMI接口的,该如何修改内核代码呢?有没有参考手册,或者patch等,请帮忙找找资料,非常感谢!
从DPI切换到HDMI是什么意思?我们已经在EVM上做到了这一点,它支持1920x1080分辨率。