This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: 基于SK-AM62A-LP E3开发板的HDMI接口点任意尺寸屏幕

Part Number: SK-AM62A-LP


基于SK-AM62A-LP E3开发板,通过HDMI接口,如何点不同分辨率的屏幕?如何更改时钟,是否可以点8bit/10bit,有没有参考资料?

以上问题,期待您的回复,非常感谢!

  • 你能解释一下你的用例吗?一般来说,您的HDMI显示器将支持一系列分辨率,您可以通过Linux命令进行查询:modetest-M tidss

  • 您好,我想知道SK-AM62A-LP支持的HDMI的限制是多少?
    我需要点类似于如下几个非标准分辨率
    8inch 1350x810@60hz pixel clock frequency=84.25Mhz 8bit
    11inch 2000x810@60Hz pixel clock frequency=117.180Mhz 8bit/10bit
    17.7inch 3400x1300@60Hz pixel clock frequency=283.5Mhz 8bit/10bit
    点亮方式
    1.不读取edid,HDMI强制输出;或者uboot启动时设置,直接可以输出?
    2.读取edid,通过读到的edid,设置对应的HDMI时序,
    以上问题,请帮忙看看,推荐些资料,非常感谢!

  • 为了达到预期,我们在AM62A上不支持HDMI。我们通过SII9022A电桥将DPI信号转换为HDMI。我相信这座桥只支持最高1920x1080分辨率。这与TI SOC无关,而是与桥接限制有关。我们的最大PCLK为165MHz,因此我们可以支持高达该PCLK的分辨率。您上面列出的分辨率不是我们测试过的,我们的EVM+SW仅在1920x1080分辨率下进行了测试。

  • 您好,

          如果我这边点最大不超过1920x1080和PCLK=165MHz的通过DPI转换为HDMI接口的,该如何修改内核代码呢?有没有参考手册,或者patch等,请帮忙找找资料,非常感谢!

  • 从DPI切换到HDMI是什么意思?我们已经在EVM上做到了这一点,它支持1920x1080分辨率。