This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x启动安卓的时候一直显示init: untracked pid xxx exited

Other Parts Discussed in Thread: TPS65910

 init: untracked pid 133 exited                                   
[   21.620727] init: untracked pid 214 exited                                   
[   26.947296] init: untracked pid 221 exited                                   
[   34.322906] init: untracked pid 228 exited                                   
[   36.742980] init: untracked pid 235 exited                                   
[   44.253082] init: untracked pid 242 exited                                   
[   46.672698] init: untracked pid 249 exited                                   
[   52.094116] init: untracked pid 256 exited                                   
[   56.513092] init: untracked pid 263 exited                                   
[   61.943115] init: untracked pid 270 exited

shell 命令也能用,但是一直打印这样的错误。是什么原因造成的呢?

  • 最后打打印信息如下:

    [    2.861938] EXT4-fs (mmcblk0p2): recovery complete                          
    [    2.870483] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode.)
    [    2.879028] VFS: Mounted root (ext4 filesystem) on device 179:2.            
    [    2.885925] Freeing init memory: 348K                                       
    [    2.927124] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom.
    [    3.025299] init: cannot open '/initlogo.rle'                               
    [    3.060882] init: cannot find '/system/bin/sgx/rc.pvr', disabling 'pvr'     
    [    3.070892] init: cannot find '/system/bin/rild', disabling 'ril-daemon'    
    [    3.108306] init: cannot find '/system/etc/install-recovery.sh', disabling '
    [    3.136657] android_usb: already disabled                                   
    [    3.141174] mtp_bind_config                                                 
    [    3.144195] adb_bind_config                                                 
    [    3.223480] adb_open                                                        
    root@android:/ # [    5.199554] init: untracked pid 64 exited                  
    [    9.030517] init: untracked pid 149 exited                                  
    [   14.677398] init: untracked pid 216 exited                                  
    [   22.002593] init: untracked pid 223 exited

  • 有完整的log吗? lcd有反应吗?

  • Starting kernel ...                                                             
                                                                                    
    Uncompressing Linux... done, booting the kernel.                                
    [    0.000000] Linux version 3.2.0 (root@ubuntu) (gcc version 4.4.3 (GCC) ) #5 5
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d  
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructie
    [    0.000000] Machine: am335xevm                                               
    [    0.000000] Memory policy: ECC disabled, Data cache writeback                
    [    0.000000] AM335X ES2.0 (sgx neon )                                         
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pa4
    [    0.000000] Kernel command line: console=ttyO0,115200n8 androidboot.console=f
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)              
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)  
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)    
    [    0.000000] Memory: 256MB = 256MB total                                      
    [    0.000000] Memory: 250172k/250172k available, 11972k reserved, 0K highmem   
    [    0.000000] Virtual kernel memory layout:                                    
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)                
    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)                
    [    0.000000]     vmalloc : 0xd0800000 - 0xff000000   ( 744 MB)                
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)                
    [    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)                
    [    0.000000]       .text : 0xc0008000 - 0xc0761000   (7524 kB)                
    [    0.000000]       .init : 0xc0761000 - 0xc07b8000   ( 348 kB)                
    [    0.000000]       .data : 0xc07b8000 - 0xc081e9f0   ( 411 kB)                
    [    0.000000]        .bss : 0xc081ea14 - 0xc09745d8   (1367 kB)                
    [    0.000000] NR_IRQS:396                                                      
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrus
    [    0.000000] Total of 128 interrupts on 1 active controller                   
    [    0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz                  
    [    0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz                           
    [    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 1s
    [    0.000000] Console: colour dummy device 80x30                               
    [    0.000152] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)          
    [    0.089233] pid_max: default: 32768 minimum: 301                             
    [    0.089355] Security Framework initialized                                   
    [    0.089416] Mount-cache hash table entries: 512                              
    [    0.089782] CPU: Testing write buffer coherency: ok                          
    [    0.089843] ftrace: allocating 21678 entries in 64 pages                     
    [    0.146026] omap_hwmod: pruss: failed to hardreset                           
    [    0.146759] print_constraints: dummy:                                        
    [    0.146972] NET: Registered protocol family 16                               
    [    0.147918] OMAP GPIO hardware version 0.1                                   
    [    0.148803] omap_mux_init: Add partition: #1: core, flags: 0                 
    [    0.149871]  omap_i2c.1: alias fck already exists                            
    [    0.150329]  omap2_mcspi.1: alias fck already exists                         
    [    0.150390]  omap2_mcspi.2: alias fck already exists                         
    [    0.150543]  edma.0: alias fck already exists                                
    [    0.150543]  edma.0: alias fck already exists                                
    [    0.150543]  edma.0: alias fck already exists                                
    [    0.158325] bio: create slab <bio-0> at 0                                    
    [    0.159149] SCSI subsystem initialized                                       
    [    0.159973] usbcore: registered new interface driver usbfs                   
    [    0.160064] usbcore: registered new interface driver hub                     
    [    0.160186] usbcore: registered new device driver usb                        
    [    0.160308] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3   
    [    0.160430] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1   
    [    0.160827] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz                   
    [    0.161926] tps65910 1-002d: JTAGREVNUM 0x0                                  
    [    0.164062] print_constraints: VRTC:                                         
    [    0.165374] print_constraints: VIO: at 1500 mV                               
    [    0.167541] print_constraints: VDD1: 600 <--> 1500 mV at 1325 mV normal      
    [    0.169708] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal      
    [    0.170593] print_constraints: VDD3: 5000 mV                                 
    [    0.171844] print_constraints: VDIG1: at 1800 mV                             
    [    0.173156] print_constraints: VDIG2: at 1800 mV                             
    [    0.174438] print_constraints: VPLL: at 1800 mV                              
    [    0.175720] print_constraints: VDAC: at 1800 mV                              
    [    0.177001] print_constraints: VAUX1: at 1800 mV                             
    [    0.178283] print_constraints: VAUX2: at 3300 mV                             
    [    0.179565] print_constraints: VAUX33: at 3300 mV                            
    [    0.180847] print_constraints: VMMC: at 3300 mV                              
    [    0.181091] tps65910 1-002d: No interrupt support, no core IRQ               
    [    0.181518] Advanced Linux Sound Architecture Driver Version 1.0.24.         
    [    0.182006] Bluetooth: Core ver 2.16                                         
    [    0.182067] NET: Registered protocol family 31                               
    [    0.182098] Bluetooth: HCI device and connection manager initialized         
    [    0.182098] Bluetooth: HCI socket layer initialized                          
    [    0.182098] Bluetooth: L2CAP socket layer initialized                        
    [    0.182128] Bluetooth: SCO socket layer initialized                          
    [    0.182312] Switching to clocksource gp timer                                
    [    0.197448] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)             
    [    0.197631] musb-hdrc musb-hdrc.0: dma type: pio                             
    [    0.197814] MUSB0 controller's USBSS revision = 4ea20800                     
    [    0.198181] musb-hdrc musb-hdrc.0: USB OTG mode controller at d083c000 using8
    [    0.198455] musb-hdrc musb-hdrc.1: dma type: pio                             
    [    0.198577] MUSB1 controller's USBSS revision = 4ea20800                     
    [    0.198669] musb-hdrc musb-hdrc.1: MUSB HDRC host driver                     
    [    0.198760] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numb1
    [    0.198883] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002    
    [    0.198883] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber1
    [    0.198913] usb usb1: Product: MUSB HDRC host driver                         
    [    0.198913] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd                     
    [    0.198913] usb usb1: SerialNumber: musb-hdrc.1                              
    [    0.199310] hub 1-0:1.0: USB hub found                                       
    [    0.199340] hub 1-0:1.0: 1 port detected                                     
    [    0.199676] musb-hdrc musb-hdrc.1: USB Host mode controller at d083e800 usin9
    [    0.200012] NET: Registered protocol family 2                                
    [    0.200195] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)   
    [    0.200531] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.200622] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)        
    [    0.200714] TCP: Hash tables configured (established 8192 bind 8192)         
    [    0.200714] TCP reno registered                                              
    [    0.200714] UDP hash table entries: 256 (order: 0, 4096 bytes)               
    [    0.200744] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)          
    [    0.200897] NET: Registered protocol family 1                                
    [    0.201171] RPC: Registered named UNIX socket transport module.              
    [    0.201171] RPC: Registered udp transport module.                            
    [    0.201171] RPC: Registered tcp transport module.                            
    [    0.201171] RPC: Registered tcp NFSv4.1 backchannel transport module.        
    [    0.201385] NetWinder Floating Point Emulator V0.97 (double precision)       
    [    0.288787] ashmem: initialized                                              
    [    0.289031] VFS: Disk quotas dquot_6.5.2                                     
    [    0.289062] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)       
    [    0.289825] fuse init (API version 7.17)                                     
    [    0.290008] msgmni has been set to 488                                       
    [    0.290924] io scheduler noop registered                                     
    [    0.290924] io scheduler deadline registered                                 
    [    0.290985] io scheduler cfq registered (default)                            
    [    0.291473] Could not set LED4 to fully on                                   
    [    0.303161] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
    [    0.965057] console [ttyO0] enabled                                          
    [    0.969146] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    [    0.976806] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    [    0.984466] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
    [    0.992065] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
    [    0.999694] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
    [    1.011871] brd: module loaded                                               
    [    1.017547] loop: module loaded                                              
    [    1.020996] i2c-core: driver [tsl2550] using legacy suspend method           
    [    1.027526] i2c-core: driver [tsl2550] using legacy resume method            
    [    1.033966] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write  
    [    1.092895] No daughter card found on AM335x EVM                             
    [    1.097747] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write  
    [    1.105194] The board is general purpose EVM in profile 0                    
    [    1.111145]  omap_hsmmc.0: alias fck already exists                          
    [    1.117187] NFC Driver for TI WiLink                                         
    [    1.121490] mtdoops: mtd device (mtddev=name/number) must be supplied        
    [    1.128601] omap2-nand driver initializing                                   
    [    1.132965] OneNAND driver initializing                                      
    [    1.137390] CAN device driver interface                                      
    [    1.141387] CAN bus driver for Bosch D_CAN controller 1.0                    
    [    1.192932] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6           
    [    1.199401] davinci_mdio davinci_mdio.0: detected phy mask ffffff7e          
    [    1.207244] davinci_mdio.0: probed                                           
    [    1.210815] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
    [    1.218231] davinci_mdio davinci_mdio.0: phy[7]: device 0:07, driver unknown
    [    1.225646] PPP generic driver version 2.4.2                                 
    [    1.230285] PPP BSD Compression module registered                            
    [    1.235229] PPP Deflate Compression module registered                        
    [    1.240600] usbcore: registered new interface driver cdc_ether               
    [    1.246765] usbcore: registered new interface driver cdc_eem                 
    [    1.252716] usbcore: registered new interface driver dm9601                  
    [    1.258575] usbcore: registered new interface driver cdc_subset              
    [    1.264831] cdc_ncm: 04-Aug-2011                                             
    [    1.268249] usbcore: registered new interface driver cdc_ncm                 
    [    1.274230] usbcore: registered new interface driver cdc_acm                 
    [    1.280151] cdc_acm: USB Abstract Control Model driver for USB modems and ISs
    [    1.288513] Initializing USB Mass Storage driver...                          
    [    1.293731] usbcore: registered new interface driver usb-storage             
    [    1.300018] USB Mass Storage support registered.                             
    [    1.304992] usbcore: registered new interface driver usbserial               
    [    1.311096] USB Serial support registered for generic                        
    [    1.316467] usb 1-1: new high-speed USB device number 2 using musb-hdrc      
    [    1.463073] usb 1-1: New USB device found, idVendor=0424, idProduct=2512     
    [    1.470092] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
    [    1.478027] hub 1-1:1.0: USB hub found                                       
    [    1.482025] hub 1-1:1.0: 2 ports detected                                    
    [    1.486877] usbcore: registered new interface driver usbserial_generic       
    [    1.493743] usbserial: USB Serial Driver core                                
    [    1.498321] USB Serial support registered for GSM modem (1-port)             
    [    1.504791] usbcore: registered new interface driver option                  
    [    1.510620] option: v0.7.2:USB Driver for GSM modems                         
    [    1.517272]  gadget: Mass Storage Function, version: 2009/09/11              
    [    1.523498]  gadget: Number of LUNs=1                                        
    [    1.527343]  lun0: LUN: removable file: (no medium)                          
    [    1.532623]  gadget: android_usb ready                                       
    [    1.536590] musb-hdrc musb-hdrc.0: MUSB HDRC host driver                     
    [    1.542175] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus numb2
    [    1.549987] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002    
    [    1.557098] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber1
    [    1.564666] usb usb2: Product: MUSB HDRC host driver                         
    [    1.569854] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd                     
    [    1.575408] usb usb2: SerialNumber: musb-hdrc.0                              
    [    1.580505] hub 2-0:1.0: USB hub found                                       
    [    1.584472] hub 2-0:1.0: 1 port detected                                     
    [    1.589050] mousedev: PS/2 mouse device common for all mice                  
    [    1.595977] using rtc device, omap_rtc, for alarms                           
    [    1.600830] omap_rtc omap_rtc: rtc core: registered omap_rtc as rtc0         
    [    1.607788] i2c /dev entries driver                                          
    [    1.611602] Linux video capture interface: v2.00                             
    [    1.616699] usbcore: registered new interface driver uvcvideo                
    [    1.622680] USB Video Class driver (1.1.1)                                   
    [    1.663635] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec             
    [    1.670135] device-mapper: uevent: version 1.0.3                             
    [    1.675170] device-mapper: ioctl: 4.22.0-ioctl (2011-10-19) initialised: dm-m
    [    1.683990] Bluetooth: HCI UART driver ver 2.2                               
    [    1.688659] Bluetooth: HCI H4 protocol initialized                           
    [    1.693664] Bluetooth: HCILL protocol initialized                            
    [    1.698577] Bluetooth: Bluetooth Driver for TI WiLink - Version 1.0          
    [    1.709442] cpuidle: using governor ladder                                   
    [    1.713897] cpuidle: using governor menu                                     
    [    1.720153] usbcore: registered new interface driver usbhid                  
    [    1.726043] usbhid: USB HID core driver                                      
    [    1.730560] logger: created 256K log 'log_main'                              
    [    1.735443] logger: created 256K log 'log_events'                            
    [    1.740447] logger: created 256K log 'log_radio'                             
    [    1.745391] logger: created 256K log 'log_system'                            
    [    1.750793] usbcore: registered new interface driver snd-usb-audio           
    [    1.758117] ALSA device list:                                                
    [    1.761199]   No soundcards found.                                           
    [    1.764801] oprofile: hardware counters not available                        
    [    1.770050] oprofile: using timer interrupt.                                 
    [    1.774688] Netfilter messages via NETLINK v0.30.                            
    [    1.779724] nf_conntrack version 0.5.0 (3908 buckets, 15632 max)             
    [    1.786376] ctnetlink v0.93: registering with nfnetlink.                     
    [    1.791992] NF_TPROXY: Transparent proxy support initialized, version 4.1.0  
    [    1.799285] NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.               
    [    1.805725] xt_time: kernel timezone is -0000                                
    [    1.810485] ip_tables: (C) 2000-2006 Netfilter Core Team                     
    [    1.816314] arp_tables: (C) 2002 David S. Miller                             
    [    1.821197] TCP cubic registered                                             
    [    1.824768] NET: Registered protocol family 10                               
    [    1.830230] Mobile IPv6                                                      
    [    1.832824] ip6_tables: (C) 2000-2006 Netfilter Core Team                    
    [    1.838714] IPv6 over IPv4 tunneling driver                                  
    [    1.843780] NET: Registered protocol family 17                               
    [    1.848449] NET: Registered protocol family 15                               
    [    1.853149] can: controller area network core (rev 20090105 abi 8)           
    [    1.859710] NET: Registered protocol family 29                               
    [    1.864379] can: raw protocol (rev 20090105)                                 
    [    1.868835] can: broadcast manager protocol (rev 20090105 t)                 
    [    1.875213] Bluetooth: RFCOMM TTY layer initialized                          
    [    1.880310] Bluetooth: RFCOMM socket layer initialized                       
    [    1.885711] Bluetooth: RFCOMM ver 1.11                                       
    [    1.889617] Bluetooth: BNEP (Ethernet Emulation) ver 1.3                     
    [    1.895172] Bluetooth: BNEP filters: protocol multicast                      
    [    1.900634] Bluetooth: HIDP (Human Interface Emulation) ver 1.2              
    [    1.906982] Registering the dns_resolver key type                            
    [    1.911956] VFP support v0.3: implementor 41 architecture 3 part 30 variant 3
    [    1.919982] ThumbEE CPU extension supported.                                 
    [    1.924499] mux: Failed to setup hwmod io irq -22                            
    [    1.930114] Power Management for AM33XX family                               
    [    1.934997] Trying to load am335x-pm-firmware.bin (60 secs timeout)          
    [    1.941650] Copied the M3 firmware to UMEM                                   
    [    1.949981] clock: disabling unused clocks to save power                     
    [    1.957153] Detected MACID=20:cd:39:d9:82:d2                                 
    [    1.962890] omap_rtc omap_rtc: setting system clock to 2000-01-01 00:00:00 U)
    [    1.972229] Waiting for root device /dev/mmcblk0p2...                        
    [    2.015899] mmc0: new high speed SDHC card at address 1234                   
    [    2.022155] mmcblk0: mmc0:1234 SA04G 3.63 GiB                                
    [    2.028930]  mmcblk0: p1 p2 p3                                               
    [    5.737548] EXT4-fs (mmcblk0p2): recovery complete                           
    [    5.746032] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. )
    [    5.754577] VFS: Mounted root (ext4 filesystem) on device 179:2.             
    [    5.761474] Freeing init memory: 348K                                        
    [    5.794006] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_.
    [    5.877746] init: cannot open '/initlogo.rle'                                
    [    5.907806] init: cannot find '/system/bin/rild', disabling 'ril-daemon'     
    [    5.981903] init: cannot find '/system/etc/install-recovery.sh', disabling ''
    [    5.994445] android_usb: already disabled                                    
    [    6.001495] mtp_bind_config                                                  
    [    6.004577] adb_bind_config                                                  
    [    6.150268] adb_open                                                         
    root@android:/ # [    6.226562] Disabling lock debugging due to kernel taint    
    [    6.278717] omaplfb: OMAPLFB_Init: OMAPLFBInit failed                        
    [    8.784881] init: untracked pid 66 exited                                    
    [   10.991088] init: untracked pid 221 exited                                   
    [   11.882934] init: untracked pid 222 exited

    网上有说是权限问题的,但是改了也没什么用。是不是第一个进程都没启动?

  • LCD没反应,不能显示。 这个板子是照着画的,之前linux系统也能跑起来,也能显示。但是安卓的有些问题。

  • 您的文件系统写到sd卡的时候,用的是root权限吗

  • 是用root做的文件系统。

    之前的sd卡可读写检查函数我给成直接跳过了,sd卡可能是只读状态。应该怎么办呢?

  • SD卡启动的话,应该是读写状态才对,请问您是对SD卡加了写保护了么?

  • 对SD卡分了三个区,boot,rootfs,data  。rootfs确实不可写,我不知道怎么加的写保护,该怎么解决呢?

  • 检查下硬件部分设计原理图,另外如果是大卡,看看是不是卡上的写保护开关打开了。

  • 应该不是硬件的原因,同样的卡,可以完整运行官方的Linux。但是跑安卓就出问题。

    是小卡,但是用了大卡套与笔记本连接,写保护锁一直没开啊。一直郁闷中。

    刚才试了试用非root用户制作SD卡,但还是同样的问题。

  • 检查下android的SD驱动初始化部分,看看是不是使能了写保护

  • 你好,我也遇到同样的问题,请问最终是怎么解决的?