This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446运行linux2.6.18很卡



各位大神好!

我在用dm6446的时候遇到下面两个问题

1. 在dm6446上移植linux2.6.18(官网下载的mvl_5_0_0_demo_lsp_setuplinux_02_00_00_140.bin)后,发现串口输入指令和反应都是一卡一卡的,比如:我输入ls指令,显示内容的时候就会卡一下,我用的编译器是:gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)

移植是没进行任何修改,只是去掉了ATA编译选项,请问这是为什么?

 

2.在配置CLK_OUT0输出时

我增加了 MUX_CFG("CLKOUT0",   1,   16,    1,   1,  1)

却发现在配置psc时没有发现DAVINCI_LPSC_CLKOUT0的定义-------------类似于davinci_psc_config(DAVINCI_GPSC_ARMDOMAIN, DAVINCI_LPSC_GPIO, 1);

而且在dm644x_setup_pinmux函数中也没发现类似于DAVINCI_LPSC_CLKOUT0(DAVINCI_LPSC_GPIO)的定义,请问我该怎么做?

 

谢谢