This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

同样的代码同样的CCS5.3属性配置,只是把输出从COFF改为ELF,导致了运行时间差别很大



情况是这样子的:硬件使用OMAPL138+射频,使用DSP内核控制MCBSP解析射频过来的数据,MCBSP每5ms产生一个EDMA中断,在中断中发出消息,用任务处理MCBSP收到的数据,在CCS环境下可以正常执行,解析数据,滤波这些操作都在2ms之内就完成了。

现在改为了用linux的平台的,这样就把dsp的输出格式从coff改为elf格式了,存储空间分配,DSP的频率,SDRAM的频率,dsp的cfg文件的配置都没有改变,只是在linux的环境下用ti提供的软件引导.out文件,虽然mcbsp依然能产生5ms的中断,但是解析数据,滤波这些操作需要15ms时间了,这样就造成了处理不过来,导致发送消息的速度大于接收的速度,会丢很多消息,处理就不正常了。

特别说明:一开始觉得两个环境下处理速度不一样,所以在两个平台下作3MBYTES的SDRAM内存空间相互拷贝,测出来的速度是一样的,这样可以说明指令处理速度都是一样的;5ms内的解析和处理只调用了TI提供的dsplib一个函数库,TI提供了coff模式和elf的格式库,这个是官方提供的,应该不会影响到运行速度的。

疑问:简单的一个没有调用库的两个函数的处理,处理之前和之后都调用硬件关闭中断功能,然后用gpio拉电平测量处理时间,在bios模式下只花了120us时间,但是在Linux模式下就需要2ms左右的时间,看了论坛里面TI工作人员的解析,只要不改变CCS编译属性的配置,只是把输出格式改为ELF,不会影响到运行速度的。但是编译出来的.out文件尺寸差别很大,COFF格式是4M,ELF格式为11M,请大侠分析分析。

PS:还有一个现象,在BIOS下面系统定时器时间很准的,但是在LINUX平台下系统定时器时间也不准了,本来20ms的定时只有几个ms了,调用的都是库代码,应用代码都是一样的。

  • 最新调试进展:一直在怀疑是不是输出的格式不一样会有不同的ccs5.3的属性配置不一样,针对这个做了一个小的测试,讲5ms消息收到之后的处理函数单独摘出来,里面的实现就是800个点的运算,没有用到函数库,只有800个点的内容拷贝和float格式的减法和乘法的运算,就是这些运算for循环800次。

    将这个函数第一次放在创建的线程里面运行,用while(1){led_on(); process();lef_off();process();}就是这样子的运行,process();函数运行完需要2ms;第二次将这个while(1){led_on(); process();lef_off();process();}就放在工程的main{}第一句话,不放在线程里面,相当于不初始化任何操作系统的东西,就是用Linux引导了一个while(1)死循环,这样测试出来process();的执行时间只需要120us,120us这个结果就是我想要的值。

    其实Linux的功能就是引导一下dsp的.out文件,dsp还是跑在实地址模式下面,调用的接口也是一样的,只是将TI的库文件对应的从coff格式改为elf格式而已,但是这个process();函数里面根本也没有调用库文件,是不是任务调度出现问题了(但是这个任务调度跟不用linux引导的任务调用函数是一样的,都是用的SYS/BIOS的接口)?

  • 感觉现在就是怀疑是否是LINUX引导造成的这个问题,可以改用CCS JTAG来引导DSP的程序,看看有没有区别。