This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.DSS supports two types of display interfaces(Display parallel interface & Two low-voltage differential signaling (LVDS) interfaces):could this two interfaces work simultaneously(same display content),or just one of them at the same time?
2.Display parallel interface:does it surpport output
A.8/10/16-Bit 4:2:2 YCrCb?
B.16-Bit 4:2:2 YCrCb?
C.16-Bit 4:4:4 RGB?
THANKS A LOT!
Hi,
Both interfaces can be driven simultaneously. In terms of output, we support RGB(16 or 24bit modes) and YUV422(BT.656/BT.1120 only).
Regards,
Lydia
Hi,
Can you review section: 12.9.1.4.1.10.4 DISPC VP BT.656 and BT.1120 Modes and see if it helps.
Regards,
Lydia