This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

主DSP 5517的EMIF (使用CS2)和从DSP HPI(非复用模式)之间通信问题,求解决。



5517 EMIF口连接到异步存储器的连接方式(16bit的数据线,20根地址线),就可以知道从DSP HPI口是16位主机接口,不是8位接口。

EMIF,BYTEMODE = 00b,ASIZE = 01b。那么host通过HPI口对从DSP的寄存器以及内存就 是每字地址产生16bit访问。那么主DSP对从DSP的寄存器访问也一样吗?

例如,reg 的字地址是0x2100,那么我通过对地址(0x400000+0x2100)读写操作就可以实现对该寄存器的读写操作,还是地址(0x400000+0x4200)的操作?

有没有5517 通过hpi口boot另一个dsp的例程,谢谢