This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM37x EVM Schematic & board reference files

Other Parts Discussed in Thread: AM3715, DM3730

Hi TI expert
能帮忙找下AM37x EVM schematic跟BOM吗 ??wiki上面貌似找不到。


EVM & Development Boards

  • EVM - AM37x EVM Schematic & board reference files are available here.
  • BeagleBoard xM available for Open Source design. community-supported platform that can be used as the basis for building more complete evelopment systems and as a target for community software baselines.
  • GEL files and configuration files for Code Composer Studio can be found here.
  • Embest DevKit8500D Evaluation board based on TI DM3730 processor supports for linux2.6.32, Android2.2 and WinCE6.0 operating systems. (DevKit8500A is also available for TI AM3715)
  • Embest SBC8530 uses POP (Package on Package) CPU/Memory chip to interface the 1GHz DM3730 processor to 512MBytes of Nand flash and 512MBytes of DDR SDRAM and features serial, 4 USB Host, USB OTG, Ethernet, WiFi/BT, Audio, TF, LCD, touch screen, DVI-D and S-Video interfaces on board, supporting for linux2.6.32, Android2.2 and WinCE6.0 operating systems.