Part Number: J721EXSOMXEVM
Hello, referring to the guide at this link, I encountered errors while attempting to create the image and flash it to the SD card.

-
What should be selected for the boot partition and rootfs partition when creating a custom SD card? Should both be from
deploy-ti/images/j721e-evm? -
Can the kernel image and device tree files simply select "Reuse kernel image and device tree files found in the selected rootfs"?
-
Will there be any impact if the
setup.shscript was not run before building the SDK with Yocto? - Is “installing SDK -> yocto to build SDK, generating deploy ti/images/j721e-evm/ -> running create sdcard.sh” the complete process of burning the image?