DM8168,采用DVRRDK3.5,通过接收网络数据解码后交给SWMS组成9画面,整u个画面均有彩条,请问是什么原因呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
[m3vpss ] *** [SWMS0] Mosaic Parameters ***
[m3vpss ]
[m3vpss ] Output FPS: 60
[m3vpss ]
[m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data | Blank |
[m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format| Frame |
[m3vpss ] ----------------------------------------------------------------------------------------------------------------------------------------------------------------------
[m3vpss ] 0 | 0 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 0, 0 | 640 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 1 | 1 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 640, 0 | 640 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 2 | 2 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 1280, 0 | 632 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 3 | 3 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 0, 360 | 640 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 4 | 4 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 640, 360 | 640 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 5 | 5 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 1280, 360 | 632 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 6 | 6 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 0, 720 | 640 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 7 | 7 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 640, 720 | 640 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
[m3vpss ] 8 | 8 | 0, 0 | 704 x 576 | 16384 / 32768 | TILED | 1280, 720 | 632 x 360 | 3840 / 0 | NON-TILED | ON | 0 | 420SP | OFF |
打印信息,测试对了下,如果将输出分辨率设置为1600x1200,正常显示