++++++++++++++++
++++++++++++++++
我输入的脚本是: cd /opt/dvr_dvr/ti816x ==> ./init.sh ==> ./load.sh 就卡在“Set Static L3 pressure for HDVPSS as High”!
我根据脚本就卡到下面的那个命令:/scripts /load_vpss.sh
现在的情况就是卡在这里 ,又找不到原因,镜像在其他板子是可以启动的!请TI的工作人员协助!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!谢谢你的回复,最终是因为dm8168芯片贴得不好导致。 现在我获取到图像,但打印的信息 总会出现这个错误:
Critical Warning : H.264 Channel:4,P frame bitsStream Buffer size:80696,exceeds BITSTREAM_P_FRAME_SIZE!
Critical Warning : H.264 Channel:0,P frame bitsStream Buffer size:125816,exceeds BITSTREAM_P_FRAME_SIZE!
.....
怎么会出现这个严重的警告?不是很懂什么意思。