This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: Android SDK 使用时出现错误

Part Number: SK-AM62

您好!

如题,SK-AM62开发板,用Android SDK刷机启动后,报出很多错误,并且无法启动(偶然可以启动成功,但是系统非常卡顿)。

错误信息很多,请参考附件文件(从uboot启动开始之后的系统log)。

能否帮忙确认是什么原因?

LOGs.txt

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • 我截取了一段问题LOG,帮忙看看:
    [ 1.904398][ T74] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports
    [ 1.913548][ T74] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports
    [ 1.994696][ T74] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports
    [ 2.004028][ T74] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports
    [ 2.023289][ T74] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@0/ports
    [ 2.032576][ T74] OF: graph: no port node found in /bus@f0000/dss@30200000/oldi-txes/oldi@1/ports
    [ 2.076889][ T1] init: Failed to copy /avb into /metadata/gsi/dsu/avb/: No such file or directory


  • 再次补充一点,使用的刷机文件是TI官网上面的bin文件:

  • 您好

    如果你不尝试,请中断 u-boot 启动并执行以下操作:

     

    env default -a; saveenv

    然后重新启动并重新刷新所有映像、让我知道。 我在我这边进行测试、在闪存和引导上没有问题。