This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Building Full Feature EtherCAT Application for AM335x ICEv2

Other Parts Discussed in Thread: SYSBIOS

我板子AM335x ICEv2,下载了最新的sysbios_ind_sdk,想要编译Building Full Feature EtherCAT Application,按照手册说明进行到到第五步,发现ecat_def.h没有TIESC_APPLICATION定义啊,是不是我哪里弄错了。谁有完整版本编译好的给我发一下啊。我邮箱007afei@163.com,谢谢。

5. Define macros in ecat_appl\EcatStack\ecat_def.h as required for your application. (a) Ensure that TIESC_HW is
set to 1. (b) For running default application, set TIESC_APPLICATION to 1 and CiA402_DEVICE to 0. For
SYSBIOS Industrial SDK 02.01.01 User Guide 35
running CiA402 application, set TIESC_APPLICATION to 0 and CiA402_DEVICE to 1.

  • ind_idk的下载网页上应该就有prebuild image  啊

  • 按照说明build之后发现如下错误:


    **** Build of configuration am335x_debug for project ecat_appl ****

    "C:\\TI\\ccsv6\\utils\\bin\\gmake" -k all
    'Building file: ../am335x_app.cfg'
    'Invoking: XDCtools'
    "C:/ti/xdctools_3_31_02_38_core/xs" --xdcpath="C:/ti/bios_6_42_02_29/packages;" xdc.tools.configuro -o configPkg -t gnu.targets.arm.A8F -p ti.platforms.evmAM3359 -r debug -c "C:/TI/ccsv6/tools/compiler/gcc-arm-none-eabi-4_8-2014q3" "../am335x_app.cfg"
    making package.mak (because of package.bld) ...
    generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
    configuring am335x_app.xa8fg from package/cfg/am335x_app_pa8fg.cfg ...
    generating custom ti.sysbios library makefile ...
    js: "C:/TI/xdctools_3_31_02_38_core/packages/xdc/cfg/Main.xs", line 48: XDC runtime error: can't find program 'am335x_app.xa8fg's linker command template file: 'C:\ti\am335x_sysbios_ind_sdk_1.1.0.10\sdk/protocols/ethercat_slave/ecat_appl/ecat_appl.xdt' along the path C:/TI/bios_6_42_02_29/packages;C:/ti/xdctools_3_31_02_38_core/packages;..;
    gmake.exe: *** [package/cfg/am335x_app_pa8fg.xdl] Error 1
    gmake.exe: *** Deleting file `package/cfg/am335x_app_pa8fg.xdl'
    gmake.exe: *** [package/cfg/am335x_app_pa8fg.xdl] Deleting file `package/cfg/am335x_app_pa8fg.h'
    gmake.exe: *** [package/cfg/am335x_app_pa8fg.xdl] Deleting file `package/cfg/am335x_app_pa8fg.c'
    js: "C:/TI/xdctools_3_31_02_38_core/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
    gmake: *** [configPkg/linker.cmd] Error 1
    gmake: Target `all' not remade because of errors.

    **** Build Finished ****

    是XDC版本有问题吗?我该怎么解决啊?

  • 你为什么用的gcc编译的,这个不对