Q:有关DAC38RF89电流的一些问题:
1.在图149(电源方案)所示的VDDDIG1电流为2.5A;
在“Electrical Characteristics - DC Specifications”(第7.5节)中时,VDDDIG1的最大电流为1.3A。
实际的VDDDIG1预期电流是多少?
2.如果我仅使用1个DAC,预期电流是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q:有关DAC38RF89电流的一些问题:
1.在图149(电源方案)所示的VDDDIG1电流为2.5A;
在“Electrical Characteristics - DC Specifications”(第7.5节)中时,VDDDIG1的最大电流为1.3A。
实际的VDDDIG1预期电流是多少?
2.如果我仅使用1个DAC,预期电流是多少?
A:数据表手册令人困惑,图149填充最大值不知道为什么。7.5节未显示所有模式在最大频率下的电流。在9GHz时,从几台设备获取的特性数据中,最坏的情况约为2.244A。我可以在1 TX模式下运行DAC来提供数据,但不能确定这是否是您所要的。如果您打算在2 TX模式下使用该器件,然后关闭一个TX通道,请发送以下信息,我们可以为您测量实验室中的电流差:LMFS设置,DACCLK速率,interpolation factor,是否使用DAC PLL,实际数据,每通道1 I / Q或2 I / Q,位数以及使用NCO的频率。
A:查看附件Power consumption for 44210 mode 1 DAC.xlsx
第一行只是NCO运行,第二行是来自JESD接口和NCO运行的70MHz tone。该表格列出了所有单独的supply rail 电流。对于在9GHz下运行的设备,这应该是最坏的情况。